<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32 SPI5 could not read data from slave in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32-SPI5-could-not-read-data-from-slave/m-p/1482947#M976</link>
    <description>&lt;P&gt;I am trying get data from SPI slave with SPI5&lt;/P&gt;&lt;P&gt;1、Slave device is PCS21125&lt;/P&gt;&lt;P&gt;2、CS is high active,Set PCSIS Bit0 to 1)&lt;/P&gt;&lt;P&gt;3、follow is MISO and clk ,but in Linux driver,read POPR return 0.&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="新建文件4.png" style="width: 800px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/185201iD063DE96689AEFA0/image-size/large?v=v2&amp;amp;px=999" role="button" title="新建文件4.png" alt="新建文件4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I want to know is anything speical need to when PCSIS Bit is set to 1。 thanks。。。。&lt;/P&gt;</description>
    <pubDate>Thu, 30 Jun 2022 16:58:02 GMT</pubDate>
    <dc:creator>zhaopingyang_sg</dc:creator>
    <dc:date>2022-06-30T16:58:02Z</dc:date>
    <item>
      <title>S32 SPI5 could not read data from slave</title>
      <link>https://community.nxp.com/t5/S32G/S32-SPI5-could-not-read-data-from-slave/m-p/1482947#M976</link>
      <description>&lt;P&gt;I am trying get data from SPI slave with SPI5&lt;/P&gt;&lt;P&gt;1、Slave device is PCS21125&lt;/P&gt;&lt;P&gt;2、CS is high active,Set PCSIS Bit0 to 1)&lt;/P&gt;&lt;P&gt;3、follow is MISO and clk ,but in Linux driver,read POPR return 0.&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="新建文件4.png" style="width: 800px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/185201iD063DE96689AEFA0/image-size/large?v=v2&amp;amp;px=999" role="button" title="新建文件4.png" alt="新建文件4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I want to know is anything speical need to when PCSIS Bit is set to 1。 thanks。。。。&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jun 2022 16:58:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-SPI5-could-not-read-data-from-slave/m-p/1482947#M976</guid>
      <dc:creator>zhaopingyang_sg</dc:creator>
      <dc:date>2022-06-30T16:58:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32 SPI5 could not read data from slave</title>
      <link>https://community.nxp.com/t5/S32G/S32-SPI5-could-not-read-data-from-slave/m-p/1485419#M1016</link>
      <description>&lt;P&gt;Hello zhaopingyang,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Is the QSPI connected, then its problem of PCS2115, because it is running ok.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 12:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-SPI5-could-not-read-data-from-slave/m-p/1485419#M1016</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-07-06T12:44:00Z</dc:date>
    </item>
  </channel>
</rss>