<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G2-VNP-RDB2 enable pfe2 in u-boot in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1324284#M96</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I use the logging capability to save the output of printe command. here is the file.&lt;/P&gt;</description>
    <pubDate>Tue, 17 Aug 2021 03:41:27 GMT</pubDate>
    <dc:creator>chjc101</dc:creator>
    <dc:date>2021-08-17T03:41:27Z</dc:date>
    <item>
      <title>S32G2-VNP-RDB2 enable pfe2 in u-boot</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1321514#M79</link>
      <description>&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;In the Ethernet Enablement Guide for RDB2 board, We use the PFE_MAC2 port in Linux, but are we able to use this port in u-boot? When I connect the board and Windows PC and using bsp with pfe hardware, the u-boot always returns "APR Retry count exceeded".&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can use the gmac port in the BSP without pfe firmware.&lt;/P&gt;&lt;P&gt;1. is u-boot able to use pfe port?&lt;/P&gt;&lt;P&gt;2. can I use gmac port in u-boot when using BSP with pfe_firmware?&lt;/P&gt;</description>
      <pubDate>Wed, 11 Aug 2021 03:48:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1321514#M79</guid>
      <dc:creator>chjc101</dc:creator>
      <dc:date>2021-08-11T03:48:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2-VNP-RDB2 enable pfe2 in u-boot</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1322529#M83</link>
      <description>&lt;P&gt;There are the output of u-boot :&lt;/P&gt;&lt;P&gt;1.When I am using BSP without PFE firmware, I could ping my PC using the GMAC port but PFE2 port.&lt;/P&gt;&lt;P&gt;2.When I am using BSP with PFE firware, I am not able to ping my PC using GMAC port or PFE2 port.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Aug 2021 09:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1322529#M83</guid>
      <dc:creator>chjc101</dc:creator>
      <dc:date>2021-08-12T09:07:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2-VNP-RDB2 enable pfe2 in u-boot</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1322673#M84</link>
      <description>&lt;P&gt;Can you please provide the full output of u-Boot "printenv" command executed immediately after an unsuccessful ping? Please use your terminal software logging capability and provide the output in the text format rather than a screen capture.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Aug 2021 13:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1322673#M84</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-08-12T13:37:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2-VNP-RDB2 enable pfe2 in u-boot</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1322871#M87</link>
      <description>&lt;P&gt;Hello Platon,&lt;/P&gt;&lt;P&gt;I attach the text file inculding the output of printe command. I am using the BSP with PFE firmware and plug the cable into u58 and u84 port separately.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Richard&lt;/P&gt;</description>
      <pubDate>Fri, 13 Aug 2021 01:43:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1322871#M87</guid>
      <dc:creator>chjc101</dc:creator>
      <dc:date>2021-08-13T01:43:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2-VNP-RDB2 enable pfe2 in u-boot</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1323084#M90</link>
      <description>&lt;P&gt;Hello Platon,&lt;/P&gt;&lt;P&gt;I find that by changing variable ethact from eth_pfeng to eth_eqos could solve the gamc problem.&lt;/P&gt;&lt;P&gt;Then the question is how to solve the "ARP Retry count exceed" problem when using PFE2 port.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Richard&lt;/P&gt;</description>
      <pubDate>Fri, 13 Aug 2021 07:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1323084#M90</guid>
      <dc:creator>chjc101</dc:creator>
      <dc:date>2021-08-13T07:53:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2-VNP-RDB2 enable pfe2 in u-boot</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1324284#M96</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I use the logging capability to save the output of printe command. here is the file.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 03:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1324284#M96</guid>
      <dc:creator>chjc101</dc:creator>
      <dc:date>2021-08-17T03:41:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2-VNP-RDB2 enable pfe2 in u-boot</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1328952#M111</link>
      <description>&lt;P&gt;It seems that the three interface of PFEMAC0 could work, but PFE_MAC2 is still not work.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 00:59:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-VNP-RDB2-enable-pfe2-in-u-boot/m-p/1328952#M111</guid>
      <dc:creator>chjc101</dc:creator>
      <dc:date>2021-08-25T00:59:57Z</dc:date>
    </item>
  </channel>
</rss>