<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic QSPI NOR memory support in Linux in S32G</title>
    <link>https://community.nxp.com/t5/S32G/QSPI-NOR-memory-support-in-Linux/m-p/1324008#M95</link>
    <description>&lt;P&gt;I am using S32g eval board and Linux bsp24, I want to to write and read from Qspi Nor memory, normally that should be supported by the mtd driver, but what I noticed is: first there is no qspi node in the dts file, second the mtd device files under /dev are not created.&lt;/P&gt;&lt;P&gt;My questions :&lt;/P&gt;&lt;P&gt;1- How is writing and reading in qspi Nor is handled ?&lt;/P&gt;&lt;P&gt;2- Can you please share basic examples for reading and writing in the QSPI Nor Memory ?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 16 Aug 2021 17:08:39 GMT</pubDate>
    <dc:creator>bou6</dc:creator>
    <dc:date>2021-08-16T17:08:39Z</dc:date>
    <item>
      <title>QSPI NOR memory support in Linux</title>
      <link>https://community.nxp.com/t5/S32G/QSPI-NOR-memory-support-in-Linux/m-p/1324008#M95</link>
      <description>&lt;P&gt;I am using S32g eval board and Linux bsp24, I want to to write and read from Qspi Nor memory, normally that should be supported by the mtd driver, but what I noticed is: first there is no qspi node in the dts file, second the mtd device files under /dev are not created.&lt;/P&gt;&lt;P&gt;My questions :&lt;/P&gt;&lt;P&gt;1- How is writing and reading in qspi Nor is handled ?&lt;/P&gt;&lt;P&gt;2- Can you please share basic examples for reading and writing in the QSPI Nor Memory ?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Aug 2021 17:08:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/QSPI-NOR-memory-support-in-Linux/m-p/1324008#M95</guid>
      <dc:creator>bou6</dc:creator>
      <dc:date>2021-08-16T17:08:39Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI NOR memory support in Linux</title>
      <link>https://community.nxp.com/t5/S32G/QSPI-NOR-memory-support-in-Linux/m-p/1326017#M102</link>
      <description>&lt;P&gt;You are using a BSP release which is very much obsolete. Consider moving to &lt;BR /&gt;the most recent BSP 29 HF1. Visit &lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32G2-REFSW-D" target="_blank" rel="noopener"&gt;this link&lt;/A&gt; to enter the SDK download procedure. See BSP 29 HF1 User Manual Section 3.2.5.2 on how to write to &lt;BR /&gt;QSPI-based MTD partitions and boot from it.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;BR /&gt;Platon&lt;/P&gt;</description>
      <pubDate>Thu, 19 Aug 2021 06:35:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/QSPI-NOR-memory-support-in-Linux/m-p/1326017#M102</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-08-19T06:35:41Z</dc:date>
    </item>
    <item>
      <title>Re: QSPI NOR memory support in Linux</title>
      <link>https://community.nxp.com/t5/S32G/QSPI-NOR-memory-support-in-Linux/m-p/1326098#M103</link>
      <description>&lt;P&gt;Thank you for for the answer, yes it is supprted in the BSP29, thank you&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Aug 2021 08:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/QSPI-NOR-memory-support-in-Linux/m-p/1326098#M103</guid>
      <dc:creator>bou6</dc:creator>
      <dc:date>2021-08-19T08:08:26Z</dc:date>
    </item>
  </channel>
</rss>