<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Gのトピックinitsram</title>
    <link>https://community.nxp.com/t5/S32G/initsram/m-p/1916886#M9421</link>
    <description>&lt;P&gt;When I was using S32G399ARDB3,bsp is 35.0, I want to start M7 bin file .But when I used command of 'initsram 0x34100000 0x700000',Console shows it is an unkown command.Why?&lt;/P&gt;</description>
    <pubDate>Thu, 25 Jul 2024 06:35:18 GMT</pubDate>
    <dc:creator>piaochunri</dc:creator>
    <dc:date>2024-07-25T06:35:18Z</dc:date>
    <item>
      <title>initsram</title>
      <link>https://community.nxp.com/t5/S32G/initsram/m-p/1916886#M9421</link>
      <description>&lt;P&gt;When I was using S32G399ARDB3,bsp is 35.0, I want to start M7 bin file .But when I used command of 'initsram 0x34100000 0x700000',Console shows it is an unkown command.Why?&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 06:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/initsram/m-p/1916886#M9421</guid>
      <dc:creator>piaochunri</dc:creator>
      <dc:date>2024-07-25T06:35:18Z</dc:date>
    </item>
    <item>
      <title>Re: initsram</title>
      <link>https://community.nxp.com/t5/S32G/initsram/m-p/1917725#M9529</link>
      <description>&lt;P&gt;Thanks for the questions&lt;/P&gt;
&lt;P&gt;I have checked the BSP and found this u-boot command seems not be enabled by default, it may be the reason of the issue you met.&lt;/P&gt;
&lt;P&gt;We do not commonly use the u-boot to boot the M7 application, If you do want to try it, you may init SRAM by using the&lt;/P&gt;
&lt;P&gt;mw.q 0x34100000 0x0 0x700000&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jul 2024 03:16:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/initsram/m-p/1917725#M9529</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-07-26T03:16:11Z</dc:date>
    </item>
  </channel>
</rss>