<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: s32g2 serial boot mode reset repeatedly</title>
    <link>https://community.nxp.com/t5/S32G/s32g2-serial-boot-mode-reset-repeatedly/m-p/1908906#M8556</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Given the description you have provided, below will be some comments on regards of your questions:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;1.&amp;nbsp;What is the reason of the S32G-VNP-RDB2 reset repeatedly in "serial boot mode",and how can I fix the problem.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;[DA]: The reason for the RDB2 being put into a reset state when in serial boot mode is related to the Standby mode itself. S32G2 standby mode exit will trigger execution of BootROM, as told under the S32G2 Reference Manual [Page 1273, S32G2 Reference Manual, Rev. 8, February 2024]:&lt;/P&gt;
&lt;P&gt;"Exit from Standby mode triggers execution of BootROM. Depending on the wakeup source, BootROM boots from either the fast&lt;BR /&gt;boot or performs a full boot, as after any reset."&lt;/P&gt;
&lt;P&gt;Since the boot mode was defined as serial, BootROM tries to look for an application under the serial interface. Given that the VR5510 was set to a non-DEBUG state, and there is no immediate code which S32G2 can run, the WDOG is not pet and then it will issue a reset.&lt;/P&gt;
&lt;P&gt;In other words, the Standby demo cannot be executed from serial boot mode, should be directly from RCON boot mode (or flash).&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;2.&amp;nbsp;&amp;nbsp;Is this STANDBY MODE DEMO not suitable for TRACE32 online debugging?&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;[DA]: As told under the previous question,&amp;nbsp;the Standby demo cannot be executed from serial boot mode, should be directly from RCON boot mode (or flash).&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Mon, 15 Jul 2024 14:38:49 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2024-07-15T14:38:49Z</dc:date>
    <item>
      <title>s32g2 serial boot mode reset repeatedly</title>
      <link>https://community.nxp.com/t5/S32G/s32g2-serial-boot-mode-reset-repeatedly/m-p/1908637#M8545</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I ran into the following issues on my S32G-VNP-RDB2 development board:&lt;BR /&gt;When I set the development board to "serial boot mode", the development board will reset repeatedly after power-on.&lt;/P&gt;&lt;P&gt;Previously, I used TRACE32 to debug STANDBY MODE DEMO provided by John.LI . I do not know whether the above problems are caused by this.&lt;/P&gt;&lt;P&gt;When I debug the same program on our S32G274A device, the device resets repeatedly when it enters STANDBY MODE. But when I power it on again, the repeat reset disappears.&lt;/P&gt;&lt;P&gt;please tell me:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;What is the reason of the S32G-VNP-RDB2 reset repeatedly in "serial boot mode",and how can I fix the problem.&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&amp;nbsp;Is this STANDBY MODE DEMO not suitable for TRACE32 online debugging?&lt;/P&gt;&lt;P&gt;Looking forward to your reply.&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="S32G-VNP-RDB2" id="S32G-VNP-RDB2"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;LI-PRODUCT title="S32G2" id="S32G2"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jul 2024 09:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g2-serial-boot-mode-reset-repeatedly/m-p/1908637#M8545</guid>
      <dc:creator>LIU_HAO</dc:creator>
      <dc:date>2024-07-15T09:57:22Z</dc:date>
    </item>
    <item>
      <title>Re: s32g2 serial boot mode reset repeatedly</title>
      <link>https://community.nxp.com/t5/S32G/s32g2-serial-boot-mode-reset-repeatedly/m-p/1908906#M8556</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Given the description you have provided, below will be some comments on regards of your questions:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;1.&amp;nbsp;What is the reason of the S32G-VNP-RDB2 reset repeatedly in "serial boot mode",and how can I fix the problem.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;[DA]: The reason for the RDB2 being put into a reset state when in serial boot mode is related to the Standby mode itself. S32G2 standby mode exit will trigger execution of BootROM, as told under the S32G2 Reference Manual [Page 1273, S32G2 Reference Manual, Rev. 8, February 2024]:&lt;/P&gt;
&lt;P&gt;"Exit from Standby mode triggers execution of BootROM. Depending on the wakeup source, BootROM boots from either the fast&lt;BR /&gt;boot or performs a full boot, as after any reset."&lt;/P&gt;
&lt;P&gt;Since the boot mode was defined as serial, BootROM tries to look for an application under the serial interface. Given that the VR5510 was set to a non-DEBUG state, and there is no immediate code which S32G2 can run, the WDOG is not pet and then it will issue a reset.&lt;/P&gt;
&lt;P&gt;In other words, the Standby demo cannot be executed from serial boot mode, should be directly from RCON boot mode (or flash).&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;2.&amp;nbsp;&amp;nbsp;Is this STANDBY MODE DEMO not suitable for TRACE32 online debugging?&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;[DA]: As told under the previous question,&amp;nbsp;the Standby demo cannot be executed from serial boot mode, should be directly from RCON boot mode (or flash).&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jul 2024 14:38:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g2-serial-boot-mode-reset-repeatedly/m-p/1908906#M8556</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-07-15T14:38:49Z</dc:date>
    </item>
    <item>
      <title>Re: s32g2 serial boot mode reset repeatedly</title>
      <link>https://community.nxp.com/t5/S32G/s32g2-serial-boot-mode-reset-repeatedly/m-p/1910469#M8769</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;Thanks for your answer. I have solved the S32G-VNP-RDB2 reset error&amp;nbsp;. I set the vr5510 in Debug Mode via connecting the J184.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 09:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g2-serial-boot-mode-reset-repeatedly/m-p/1910469#M8769</guid>
      <dc:creator>LIU_HAO</dc:creator>
      <dc:date>2024-07-17T09:10:35Z</dc:date>
    </item>
  </channel>
</rss>