<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G3 M7 Encounters Hardfault Exception When Calling a Large External Library in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-M7-Encounters-Hardfault-Exception-When-Calling-a-Large/m-p/1908312#M8534</link>
    <description>&lt;P&gt;Hi, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235130"&gt;@XD&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the post and sorry for the delay.&lt;/P&gt;
&lt;P&gt;Regarding the memory information for the specific examples, you may refer to the ld file under project settings.&lt;/P&gt;
&lt;P&gt;Since you were allocating large memories for your specific array, not sure of your allocation method, but it is possible that specific sections(stack/data/etc.) may be overlapped. You may have to compute the actually size and re-arrange the memory settings via the ld file.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
    <pubDate>Mon, 15 Jul 2024 05:19:27 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2024-07-15T05:19:27Z</dc:date>
    <item>
      <title>S32G3 M7 Encounters Hardfault Exception When Calling a Large External Library</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-M7-Encounters-Hardfault-Exception-When-Calling-a-Large/m-p/1905608#M8380</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using the M7 Linflexd_Uart_IP_Example project to test the M core's performance on the S32G3 goldbox. When running a benchmark function from an external library, the function attempts to allocate a large array, which triggers a hardfault exception. The hardfault handler indicates this by turning on an LED.&lt;/P&gt;&lt;P&gt;I need help with:&lt;/P&gt;&lt;P&gt;1. Understanding the memory restrictions for the M7 Linflexd_Uart_IP_Example project.&lt;BR /&gt;2. Recommendations for increasing the memory allocation to prevent the hardfault exception.&lt;BR /&gt;3. Best practices for handling large memory allocations on the S32G3 M7.&lt;/P&gt;&lt;P&gt;Thank you for your assistance,&lt;/P&gt;&lt;P&gt;XD&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jul 2024 22:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-M7-Encounters-Hardfault-Exception-When-Calling-a-Large/m-p/1905608#M8380</guid>
      <dc:creator>XD</dc:creator>
      <dc:date>2024-07-10T22:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 M7 Encounters Hardfault Exception When Calling a Large External Library</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-M7-Encounters-Hardfault-Exception-When-Calling-a-Large/m-p/1908312#M8534</link>
      <description>&lt;P&gt;Hi, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235130"&gt;@XD&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the post and sorry for the delay.&lt;/P&gt;
&lt;P&gt;Regarding the memory information for the specific examples, you may refer to the ld file under project settings.&lt;/P&gt;
&lt;P&gt;Since you were allocating large memories for your specific array, not sure of your allocation method, but it is possible that specific sections(stack/data/etc.) may be overlapped. You may have to compute the actually size and re-arrange the memory settings via the ld file.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jul 2024 05:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-M7-Encounters-Hardfault-Exception-When-Calling-a-Large/m-p/1908312#M8534</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-07-15T05:19:27Z</dc:date>
    </item>
  </channel>
</rss>