<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: S32G2 load dtb</title>
    <link>https://community.nxp.com/t5/S32G/S32G2-load-dtb/m-p/1907146#M8429</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Both DTB/DTS will be used. When booting, TF-A/uboot will use the TF-A DTS/DTB, when uboot passes the control to the kernel, the kernel will use its own DTB/DTS. There is no conflict between both.&lt;/P&gt;
&lt;P&gt;Both DTB/DTS should be configured accordingly, if not when uboot passes control to the kernel, devices might not be available to the kernel itself.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Fri, 12 Jul 2024 14:24:05 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2024-07-12T14:24:05Z</dc:date>
    <item>
      <title>S32G2 load dtb</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-load-dtb/m-p/1906259#M8391</link>
      <description>&lt;P&gt;I got dts both in ATF and in kernal.When the board boots,Which dtb it will actually use?Or it will load both? Thank u.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jul 2024 11:00:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-load-dtb/m-p/1906259#M8391</guid>
      <dc:creator>piaochunri</dc:creator>
      <dc:date>2024-07-11T11:00:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 load dtb</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-load-dtb/m-p/1906505#M8394</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Both DTB's will be used at the end, but the one that is available under the&amp;nbsp;root partition of the SD card should be the Kernel one.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jul 2024 16:56:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-load-dtb/m-p/1906505#M8394</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-07-11T16:56:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 load dtb</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-load-dtb/m-p/1906848#M8422</link>
      <description>Sorry，I can not understand well and could you describe it more detailed.I can find the same device in DTS both in ATF and kernal. Do they conflict with each other?</description>
      <pubDate>Fri, 12 Jul 2024 07:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-load-dtb/m-p/1906848#M8422</guid>
      <dc:creator>piaochunri</dc:creator>
      <dc:date>2024-07-12T07:19:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 load dtb</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-load-dtb/m-p/1907146#M8429</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Both DTB/DTS will be used. When booting, TF-A/uboot will use the TF-A DTS/DTB, when uboot passes the control to the kernel, the kernel will use its own DTB/DTS. There is no conflict between both.&lt;/P&gt;
&lt;P&gt;Both DTB/DTS should be configured accordingly, if not when uboot passes control to the kernel, devices might not be available to the kernel itself.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jul 2024 14:24:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-load-dtb/m-p/1907146#M8429</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-07-12T14:24:05Z</dc:date>
    </item>
  </channel>
</rss>