<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: goldvip example error</title>
    <link>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459691#M821</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The SD card must be left inserted in the device. It contains the rootfs for the Linux BSP and the kernel.&lt;/P&gt;&lt;P&gt;Vlad&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 18 May 2022 04:53:02 GMT</pubDate>
    <dc:creator>nxf45013</dc:creator>
    <dc:date>2022-05-18T04:53:02Z</dc:date>
    <item>
      <title>goldvip example error</title>
      <link>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459224#M813</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="youngdae_0-1652777870665.png" style="width: 663px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/179998i10D36B17B220DFE8/image-dimensions/663x335?v=v2" width="663" height="335" role="button" title="youngdae_0-1652777870665.png" alt="youngdae_0-1652777870665.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Put the fsl-image-goldvip-s32g274ardb2.sdcard file of goldVIP-1.1.0-binaries into the SD card and stop while uboot is running and run write_goldvip_images was performed.&lt;/P&gt;&lt;P&gt;After all the binaries are written, power off the board, configure the DIP switches for NOR&lt;BR /&gt;Flash Boot mode (set SW4.7 to OFF) and then power on the board.&lt;/P&gt;&lt;P&gt;But an error occurred as shown in the figure above.&lt;/P&gt;&lt;P&gt;ERROR: Error: s32_io_setup failed&lt;/P&gt;&lt;P&gt;PANIC at PC : 0x0000000034306858&lt;/P&gt;&lt;P&gt;I don't know why.&lt;/P&gt;</description>
      <pubDate>Tue, 17 May 2022 09:02:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459224#M813</guid>
      <dc:creator>youngdae</dc:creator>
      <dc:date>2022-05-17T09:02:57Z</dc:date>
    </item>
    <item>
      <title>Re: goldvip example error</title>
      <link>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459301#M816</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;This error is usually encountered when the ATF can't read from the SD card. (you can try to remove it and reboot from flash, the same error will occur).&lt;/P&gt;
&lt;P&gt;Could you try a different SD card? There seems to be some kind of an issue with the one you are using.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Vlad&lt;/P&gt;</description>
      <pubDate>Tue, 17 May 2022 10:41:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459301#M816</guid>
      <dc:creator>nxf45013</dc:creator>
      <dc:date>2022-05-17T10:41:16Z</dc:date>
    </item>
    <item>
      <title>Re: goldvip example error</title>
      <link>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459563#M818</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;Thank you for reply.&lt;/P&gt;&lt;P&gt;It works fine when booting from the sd card.&lt;BR /&gt;After writing to flash with the sd card, remove the sd card and boot from flash, an error occurs.&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 00:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459563#M818</guid>
      <dc:creator>youngdae</dc:creator>
      <dc:date>2022-05-18T00:30:37Z</dc:date>
    </item>
    <item>
      <title>Re: goldvip example error</title>
      <link>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459691#M821</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The SD card must be left inserted in the device. It contains the rootfs for the Linux BSP and the kernel.&lt;/P&gt;&lt;P&gt;Vlad&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 04:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459691#M821</guid>
      <dc:creator>nxf45013</dc:creator>
      <dc:date>2022-05-18T04:53:02Z</dc:date>
    </item>
    <item>
      <title>Re: goldvip example error</title>
      <link>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459964#M826</link>
      <description>&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 10:52:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/goldvip-example-error/m-p/1459964#M826</guid>
      <dc:creator>youngdae</dc:creator>
      <dc:date>2022-05-18T10:52:35Z</dc:date>
    </item>
  </channel>
</rss>