<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Help Needed: S32G-VNP-RDB2 Board Power and Boot Issues After Flashing IVT Blob</title>
    <link>https://community.nxp.com/t5/S32G/Help-Needed-S32G-VNP-RDB2-Board-Power-and-Boot-Issues-After/m-p/1902347#M7632</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm seeking help with an issue I'm facing on my S32G-VNP-RDB2 board. Here's a detailed description of the problem:&lt;/P&gt;&lt;P&gt;&amp;nbsp;Issue Description:&lt;BR /&gt;1. **Boot Issue**: During the QSPI boot configuration, only the M7 core is booting, and Linux is not starting. However, when I configure the board for SD card boot, I can see the Linux boot log on the serial port.&lt;BR /&gt;2. **Flashing Attempt**: Based on community suggestions, I tried to boot Linux from QSPI using fin.bin. However, I mistakenly created an IVT blob with the fip.s32 image (intended for SD card) and flashed it. After this, the board stopped responding.&lt;BR /&gt;3. **Power Supply Check**: I checked the power supply with a multimeter. TP6 shows a 12V power output, but TP38 indicates no output from the IC "MVR5510AMDAHES".&lt;/P&gt;&lt;P&gt;Current State:&lt;BR /&gt;- The board shows no LED indicators when powered on.&lt;BR /&gt;- There is no response from the board when I try to flash it again.&lt;BR /&gt;- The power supply check revealed TP6 is at 12V, but TP38 has no output.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Request for Assistance:&lt;BR /&gt;1. Enable Pin Configuration: Can anyone provide details on the enable pin for the MVR5510AMDAHES IC? Is there a specific configuration or voltage required?&lt;BR /&gt;2. Recovery Procedure: Is there a recommended procedure to recover the board from this state? Can the board be recovered through USB recovery mode or any other method?&lt;BR /&gt;3. Firmware Guidance: Could someone share a known good firmware image or guide me through the correct process to reflash the board?&lt;/P&gt;&lt;P&gt;Any guidance or suggestions to help resolve this issue would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you in advance for your assistance!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sarathi&lt;/P&gt;</description>
    <pubDate>Mon, 08 Jul 2024 13:47:00 GMT</pubDate>
    <dc:creator>SARATHI_22</dc:creator>
    <dc:date>2024-07-08T13:47:00Z</dc:date>
    <item>
      <title>Help Needed: S32G-VNP-RDB2 Board Power and Boot Issues After Flashing IVT Blob</title>
      <link>https://community.nxp.com/t5/S32G/Help-Needed-S32G-VNP-RDB2-Board-Power-and-Boot-Issues-After/m-p/1902347#M7632</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm seeking help with an issue I'm facing on my S32G-VNP-RDB2 board. Here's a detailed description of the problem:&lt;/P&gt;&lt;P&gt;&amp;nbsp;Issue Description:&lt;BR /&gt;1. **Boot Issue**: During the QSPI boot configuration, only the M7 core is booting, and Linux is not starting. However, when I configure the board for SD card boot, I can see the Linux boot log on the serial port.&lt;BR /&gt;2. **Flashing Attempt**: Based on community suggestions, I tried to boot Linux from QSPI using fin.bin. However, I mistakenly created an IVT blob with the fip.s32 image (intended for SD card) and flashed it. After this, the board stopped responding.&lt;BR /&gt;3. **Power Supply Check**: I checked the power supply with a multimeter. TP6 shows a 12V power output, but TP38 indicates no output from the IC "MVR5510AMDAHES".&lt;/P&gt;&lt;P&gt;Current State:&lt;BR /&gt;- The board shows no LED indicators when powered on.&lt;BR /&gt;- There is no response from the board when I try to flash it again.&lt;BR /&gt;- The power supply check revealed TP6 is at 12V, but TP38 has no output.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Request for Assistance:&lt;BR /&gt;1. Enable Pin Configuration: Can anyone provide details on the enable pin for the MVR5510AMDAHES IC? Is there a specific configuration or voltage required?&lt;BR /&gt;2. Recovery Procedure: Is there a recommended procedure to recover the board from this state? Can the board be recovered through USB recovery mode or any other method?&lt;BR /&gt;3. Firmware Guidance: Could someone share a known good firmware image or guide me through the correct process to reflash the board?&lt;/P&gt;&lt;P&gt;Any guidance or suggestions to help resolve this issue would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you in advance for your assistance!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Sarathi&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jul 2024 13:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Help-Needed-S32G-VNP-RDB2-Board-Power-and-Boot-Issues-After/m-p/1902347#M7632</guid>
      <dc:creator>SARATHI_22</dc:creator>
      <dc:date>2024-07-08T13:47:00Z</dc:date>
    </item>
  </channel>
</rss>