<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Wrong JEDEC id read in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Wrong-JEDEC-id-read/m-p/1449750#M744</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Im having trouble to read from QSPI NOR Flash on our custom board. We are using S32G274A with MX66UW1G45G (which is mainly the same as MX25UW51245G found on RDB2 just bigger as far as I know).&lt;/P&gt;&lt;P&gt;Problem is when trying to "sf probe" I get "Unrecognized JEDEC id: 84, 83, 7f". Flash obviously responded to command 0x9F (Read ID) but it responded with wrong ID. Correct ID for this chip is 0xC2813B.&lt;/P&gt;&lt;P&gt;When using S32FlashTool everything is ok, also when trying to read ID from CM7 application also it reads correct JEDEC ID. Problem only occures in u-boot (im using LinuxBSP31).&lt;/P&gt;&lt;P&gt;I did added new flash info into spi-nor-ids.c but with correct ID not this one that it reads wrongly. If I add it with wrong ID later all reads are wrong.&lt;/P&gt;&lt;P&gt;What could be a problem?&lt;/P&gt;</description>
    <pubDate>Wed, 27 Apr 2022 07:58:35 GMT</pubDate>
    <dc:creator>st_ra</dc:creator>
    <dc:date>2022-04-27T07:58:35Z</dc:date>
    <item>
      <title>Wrong JEDEC id read</title>
      <link>https://community.nxp.com/t5/S32G/Wrong-JEDEC-id-read/m-p/1449750#M744</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Im having trouble to read from QSPI NOR Flash on our custom board. We are using S32G274A with MX66UW1G45G (which is mainly the same as MX25UW51245G found on RDB2 just bigger as far as I know).&lt;/P&gt;&lt;P&gt;Problem is when trying to "sf probe" I get "Unrecognized JEDEC id: 84, 83, 7f". Flash obviously responded to command 0x9F (Read ID) but it responded with wrong ID. Correct ID for this chip is 0xC2813B.&lt;/P&gt;&lt;P&gt;When using S32FlashTool everything is ok, also when trying to read ID from CM7 application also it reads correct JEDEC ID. Problem only occures in u-boot (im using LinuxBSP31).&lt;/P&gt;&lt;P&gt;I did added new flash info into spi-nor-ids.c but with correct ID not this one that it reads wrongly. If I add it with wrong ID later all reads are wrong.&lt;/P&gt;&lt;P&gt;What could be a problem?&lt;/P&gt;</description>
      <pubDate>Wed, 27 Apr 2022 07:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Wrong-JEDEC-id-read/m-p/1449750#M744</guid>
      <dc:creator>st_ra</dc:creator>
      <dc:date>2022-04-27T07:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: Wrong JEDEC id read</title>
      <link>https://community.nxp.com/t5/S32G/Wrong-JEDEC-id-read/m-p/1603697#M2287</link>
      <description>&lt;P&gt;Hi st_ra,&lt;/P&gt;&lt;P&gt;Are you able to resolve this issue ?&lt;/P&gt;</description>
      <pubDate>Wed, 22 Feb 2023 12:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Wrong-JEDEC-id-read/m-p/1603697#M2287</guid>
      <dc:creator>yellapu_anishkh</dc:creator>
      <dc:date>2023-02-22T12:41:54Z</dc:date>
    </item>
    <item>
      <title>Re: Wrong JEDEC id read</title>
      <link>https://community.nxp.com/t5/S32G/Wrong-JEDEC-id-read/m-p/1803660#M5885</link>
      <description>&lt;P&gt;pls check the follow.decrease qspinor clock to try again&lt;/P&gt;&lt;P&gt;doc&amp;amp;project&amp;amp;patch&amp;amp;script explain to support GD qspi nor in lauterbach, flash tool,ivt,fls mcal, fls bootloader and linux &lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-ADD-GDFLASH-SUPPORT/ta-p/1763551" target="_blank"&gt;https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-ADD-GDFLASH-SUPPORT/ta-p/1763551&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Feb 2024 20:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Wrong-JEDEC-id-read/m-p/1803660#M5885</guid>
      <dc:creator>Johnli</dc:creator>
      <dc:date>2024-02-07T20:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: Wrong JEDEC id read</title>
      <link>https://community.nxp.com/t5/S32G/Wrong-JEDEC-id-read/m-p/1803821#M5889</link>
      <description>&lt;P&gt;&amp;nbsp; &amp;nbsp;Doc written by Chinese, let me explain it, qspinor datasheet normally require to use low clock to read id, such as 133Mhz or 160Mhz, but our default bsp use 200Mhz, even the default qspi nor on rdb board can pass it, but other qspinor normally cannot pass it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;in the doc, we explain how to change linux driver to decrease qspi nor clock to 133Mhz to solve it, you can refer to change to uboot.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Feb 2024 02:40:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Wrong-JEDEC-id-read/m-p/1803821#M5889</guid>
      <dc:creator>Johnli</dc:creator>
      <dc:date>2024-02-08T02:40:02Z</dc:date>
    </item>
  </channel>
</rss>