<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32G3_Resourceconflict between Bootloader,M core and A core</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-Resourceconflict-between-Bootloader-M-core-and-A-core/m-p/1898387#M7425</link>
    <description>&lt;P&gt;We are working on S32G399RDB3 board .&lt;/P&gt;&lt;P&gt;The bootloader is multicore configured .RM enabled and Rm_Init is done in SysDal Deinit list.&lt;/P&gt;&lt;P&gt;We are using both M core and A core , initially both cores were booting successfully.&lt;/P&gt;&lt;P&gt;But now we are facing two scenarios&lt;/P&gt;&lt;P&gt;1.From M core side we are using PFE and LLCE CAN and as we have to use ethernet on A core side we enabled PFE and&amp;nbsp; LLCE enabled for CAN from A core side. But after this we are observing Kernel panicking.&lt;/P&gt;&lt;P&gt;2.if we enable QSPI in A core, M core will run but A core is going to kernel panicking&lt;/P&gt;&lt;P&gt;Now one document from&amp;nbsp; NXP&amp;nbsp;&lt;STRONG&gt;&lt;SPAN class=""&gt;S32G_PFE_Master_Slave_Simple_Demo_V2_2023_5_23&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN class=""&gt;&amp;nbsp;says that to avoid resource conflict we have to do the Port and MCU initilaization from bootloader and not from M core application.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;So I would like to understand that do we have to handle the port and mcu initializations in bootloader to avoid the above&amp;nbsp; mentioned conflicts.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 03 Jul 2024 12:08:51 GMT</pubDate>
    <dc:creator>kavyapk</dc:creator>
    <dc:date>2024-07-03T12:08:51Z</dc:date>
    <item>
      <title>S32G3_Resourceconflict between Bootloader,M core and A core</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-Resourceconflict-between-Bootloader-M-core-and-A-core/m-p/1898387#M7425</link>
      <description>&lt;P&gt;We are working on S32G399RDB3 board .&lt;/P&gt;&lt;P&gt;The bootloader is multicore configured .RM enabled and Rm_Init is done in SysDal Deinit list.&lt;/P&gt;&lt;P&gt;We are using both M core and A core , initially both cores were booting successfully.&lt;/P&gt;&lt;P&gt;But now we are facing two scenarios&lt;/P&gt;&lt;P&gt;1.From M core side we are using PFE and LLCE CAN and as we have to use ethernet on A core side we enabled PFE and&amp;nbsp; LLCE enabled for CAN from A core side. But after this we are observing Kernel panicking.&lt;/P&gt;&lt;P&gt;2.if we enable QSPI in A core, M core will run but A core is going to kernel panicking&lt;/P&gt;&lt;P&gt;Now one document from&amp;nbsp; NXP&amp;nbsp;&lt;STRONG&gt;&lt;SPAN class=""&gt;S32G_PFE_Master_Slave_Simple_Demo_V2_2023_5_23&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN class=""&gt;&amp;nbsp;says that to avoid resource conflict we have to do the Port and MCU initilaization from bootloader and not from M core application.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;So I would like to understand that do we have to handle the port and mcu initializations in bootloader to avoid the above&amp;nbsp; mentioned conflicts.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 12:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-Resourceconflict-between-Bootloader-M-core-and-A-core/m-p/1898387#M7425</guid>
      <dc:creator>kavyapk</dc:creator>
      <dc:date>2024-07-03T12:08:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3_Resourceconflict between Bootloader,M core and A core</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-Resourceconflict-between-Bootloader-M-core-and-A-core/m-p/1898439#M7428</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;In general, all the resources being shared with multiple cores are to be initialized under the bootloader, to prevent multiple initializations under the system itself (once per core we might say).&lt;/P&gt;
&lt;P&gt;An explanation is provided under the following community knowledge base:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-Bootloader-Customzition/ta-p/1519838" target="_blank"&gt;S32G Bootloader Customzition - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In which different examples are provided and general recommendations. This document will not cover all the related resource conflicts that could exist under S32G platform but will provide a general guideline for them.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 14:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-Resourceconflict-between-Bootloader-M-core-and-A-core/m-p/1898439#M7428</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-07-03T14:25:19Z</dc:date>
    </item>
  </channel>
</rss>