<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: S32G3 Linux BSP 38.0 linuxptp package issue</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1896388#M7392</link>
    <description>&lt;P&gt;thank you, that was very helpful.&lt;/P&gt;</description>
    <pubDate>Mon, 01 Jul 2024 06:05:51 GMT</pubDate>
    <dc:creator>Sungbhin-Oh</dc:creator>
    <dc:date>2024-07-01T06:05:51Z</dc:date>
    <item>
      <title>S32G3 Linux BSP 38.0 linuxptp package issue</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1895104#M7350</link>
      <description>&lt;P&gt;Hi, community.&lt;/P&gt;&lt;P&gt;I am using an &lt;STRONG&gt;S32G-VNP-RDB3&lt;/STRONG&gt; board, building &lt;STRONG&gt;Linux BSP 38.0&lt;/STRONG&gt; to develop PFE and PTP.&lt;/P&gt;&lt;P&gt;According to the user manual, linuxptp tools (&lt;EM&gt;ethtool, ptp4l&lt;/EM&gt;, etc) are installed by default. However, when I run &lt;EM&gt;ethtool&lt;/EM&gt; or &lt;EM&gt;ptp4l&lt;/EM&gt; command on my Linux BSP, it outputs command not found.&lt;/P&gt;&lt;P&gt;I built BSP using YOCTO as follwed the user manual, is there something extra I need to do for linuxptp?&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 10:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1895104#M7350</guid>
      <dc:creator>Sungbhin-Oh</dc:creator>
      <dc:date>2024-06-27T10:48:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 Linux BSP 38.0 linuxptp package issue</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1895227#M7354</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;PTP is indeed available by default, but only under the&amp;nbsp;&lt;EM&gt;auto&lt;/EM&gt; image, as told under the BSP38.0 User Manual:&lt;/P&gt;
&lt;P&gt;"The linuxptp tools are installed by default in fsl-image-auto".&lt;/P&gt;
&lt;P&gt;Did you build the&amp;nbsp;&lt;EM&gt;fsl-image-auto&lt;/EM&gt; image? As for recommendations, we can recommend using the prebuilt images provided by NXP (in a *tgz file) since all features available under the auto image should be ready to be used.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 14:14:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1895227#M7354</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-06-27T14:14:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 Linux BSP 38.0 linuxptp package issue</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1895894#M7370</link>
      <description>&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;I re-build with 'fsl-image-auto' instead of 'base' and the PTP feature is enabled.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Oh, and one more thing, can you tell me how to set up the prebuilt tgz file on the SD card, and is the SJA1110 switch firmware included in this prebuilt tgz file?&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 11:23:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1895894#M7370</guid>
      <dc:creator>Sungbhin-Oh</dc:creator>
      <dc:date>2024-06-28T11:23:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 Linux BSP 38.0 linuxptp package issue</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1895989#M7373</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback.&lt;/P&gt;
&lt;P&gt;For the *.tgz files, you need to decompress them and you will find several folders which relate to the different NXP reference boards. Once you find the NXP reference board you have (or your board is based on) and you will find an *.sdcard file which is the file you need to use:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DanielAguirre_0-1719585449160.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/286257i3CB2CC517CE3393C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DanielAguirre_0-1719585449160.png" alt="DanielAguirre_0-1719585449160.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;As for the SJA1110, we understand that it is not. The FW for SJA1110 is available under the GoldVIP package. Under the NXP reference boards, the SJA1110 is preloaded with a binary, which does not require any additional loading unless the configuration on the SJA1110 needs to be changed.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 14:38:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1895989#M7373</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-06-28T14:38:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 Linux BSP 38.0 linuxptp package issue</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1896388#M7392</link>
      <description>&lt;P&gt;thank you, that was very helpful.&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 06:05:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-Linux-BSP-38-0-linuxptp-package-issue/m-p/1896388#M7392</guid>
      <dc:creator>Sungbhin-Oh</dc:creator>
      <dc:date>2024-07-01T06:05:51Z</dc:date>
    </item>
  </channel>
</rss>