<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32G2 - maximum bandwidth Cortex M7 to the internal system RAM ? in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G2-maximum-bandwidth-Cortex-M7-to-the-internal-system-RAM/m-p/1448421#M739</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;customer ask about the maximum available bandwidth from the Cortex M7 cores to the internal system RAM (not the TCM) ? &lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;thanks&lt;/P&gt;
&lt;P&gt;Jochen&lt;/P&gt;</description>
    <pubDate>Mon, 25 Apr 2022 09:33:59 GMT</pubDate>
    <dc:creator>jochengerster</dc:creator>
    <dc:date>2022-04-25T09:33:59Z</dc:date>
    <item>
      <title>S32G2 - maximum bandwidth Cortex M7 to the internal system RAM ?</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-maximum-bandwidth-Cortex-M7-to-the-internal-system-RAM/m-p/1448421#M739</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;customer ask about the maximum available bandwidth from the Cortex M7 cores to the internal system RAM (not the TCM) ? &lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;thanks&lt;/P&gt;
&lt;P&gt;Jochen&lt;/P&gt;</description>
      <pubDate>Mon, 25 Apr 2022 09:33:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-maximum-bandwidth-Cortex-M7-to-the-internal-system-RAM/m-p/1448421#M739</guid>
      <dc:creator>jochengerster</dc:creator>
      <dc:date>2022-04-25T09:33:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 - maximum bandwidth Cortex M7 to the internal system RAM ?</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-maximum-bandwidth-Cortex-M7-to-the-internal-system-RAM/m-p/1448731#M740</link>
      <description>&lt;P&gt;Hello Jochengerster,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The S32G have and internal &lt;SPAN class=""&gt;Standby S&lt;SPAN class="highlight selected appended"&gt;RAM&lt;/SPAN&gt; with ECC&amp;nbsp; of 32KB.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Apr 2022 20:27:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-maximum-bandwidth-Cortex-M7-to-the-internal-system-RAM/m-p/1448731#M740</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-04-25T20:27:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 - maximum bandwidth Cortex M7 to the internal system RAM ?</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-maximum-bandwidth-Cortex-M7-to-the-internal-system-RAM/m-p/1449040#M742</link>
      <description>&lt;P&gt;Thanks for your reply - but actually the question was what is the max throughput (bandwidth) of the M7 when accessing the system RAM (x Mbit/sec)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Apr 2022 08:10:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-maximum-bandwidth-Cortex-M7-to-the-internal-system-RAM/m-p/1449040#M742</guid>
      <dc:creator>jochengerster</dc:creator>
      <dc:date>2022-04-26T08:10:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 - maximum bandwidth Cortex M7 to the internal system RAM ?</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-maximum-bandwidth-Cortex-M7-to-the-internal-system-RAM/m-p/1449250#M743</link>
      <description>&lt;P&gt;Hi jochengerster,&lt;/P&gt;
&lt;P&gt;Theoretical maximum bandwidth can not be achieved in real device due to internal&lt;/P&gt;
&lt;P&gt;buses and arbiters limitations. The total memory bandwidth in use (read+write) is around 480 MB/s which would make sense as we associate it with the bandwidth used by the framebuffer being displayed.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Apr 2022 13:37:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-maximum-bandwidth-Cortex-M7-to-the-internal-system-RAM/m-p/1449250#M743</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-04-26T13:37:24Z</dc:date>
    </item>
  </channel>
</rss>