<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using a watchdog in the uboot does not take effect in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Using-a-watchdog-in-the-uboot-does-not-take-effect/m-p/1891756#M7289</link>
    <description>&lt;P&gt;I am using the S32G platform, I have used several BSP versions to try such as BSP34, in the kernel according to the above operation watchdog is normal, in the uboot watchdog did not reset the system?&lt;/P&gt;</description>
    <pubDate>Fri, 21 Jun 2024 01:56:06 GMT</pubDate>
    <dc:creator>shiyiheng</dc:creator>
    <dc:date>2024-06-21T01:56:06Z</dc:date>
    <item>
      <title>Using a watchdog in the uboot does not take effect</title>
      <link>https://community.nxp.com/t5/S32G/Using-a-watchdog-in-the-uboot-does-not-take-effect/m-p/1891018#M7280</link>
      <description>&lt;P&gt;I want to use a watchdog under uboot, but the watchdog doesn't work, the command is as follows&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="shiyiheng_0-1718854066596.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/284975i077BB114B12844A7/image-size/medium?v=v2&amp;amp;px=400" alt="shiyiheng_0-1718854066596.png" title="shiyiheng_0-1718854066596.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Do you need any other configuration?&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 03:29:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-a-watchdog-in-the-uboot-does-not-take-effect/m-p/1891018#M7280</guid>
      <dc:creator>shiyiheng</dc:creator>
      <dc:date>2024-06-20T03:29:20Z</dc:date>
    </item>
    <item>
      <title>Re: Using a watchdog in the uboot does not take effect</title>
      <link>https://community.nxp.com/t5/S32G/Using-a-watchdog-in-the-uboot-does-not-take-effect/m-p/1891693#M7287</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232104"&gt;@shiyiheng&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;Could you please help me with your information about processor and BSP version?&lt;BR /&gt;Additionally, are you trying any guides or manuals as reference to use the watchdog?&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 22:17:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-a-watchdog-in-the-uboot-does-not-take-effect/m-p/1891693#M7287</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2024-06-20T22:17:03Z</dc:date>
    </item>
    <item>
      <title>Re: Using a watchdog in the uboot does not take effect</title>
      <link>https://community.nxp.com/t5/S32G/Using-a-watchdog-in-the-uboot-does-not-take-effect/m-p/1891756#M7289</link>
      <description>&lt;P&gt;I am using the S32G platform, I have used several BSP versions to try such as BSP34, in the kernel according to the above operation watchdog is normal, in the uboot watchdog did not reset the system?&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jun 2024 01:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-a-watchdog-in-the-uboot-does-not-take-effect/m-p/1891756#M7289</guid>
      <dc:creator>shiyiheng</dc:creator>
      <dc:date>2024-06-21T01:56:06Z</dc:date>
    </item>
    <item>
      <title>Re: Using a watchdog in the uboot does not take effect</title>
      <link>https://community.nxp.com/t5/S32G/Using-a-watchdog-in-the-uboot-does-not-take-effect/m-p/1892306#M7295</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232104"&gt;@shiyiheng&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have you tried any modifications on Uboot build process?&lt;BR /&gt;It seems that the watchdog requires a specific configuration on Uboot to enable and set the time. This configuration should be enabled by default on that BSP version; however, I'm still working with the team to confirm that.&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jun 2024 18:35:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Using-a-watchdog-in-the-uboot-does-not-take-effect/m-p/1892306#M7295</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2024-06-21T18:35:12Z</dc:date>
    </item>
  </channel>
</rss>