<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: How to USE UART1 (dev/ttyLF1) in Linux (A-Core) With BSP41.0</title>
    <link>https://community.nxp.com/t5/S32G/How-to-USE-UART1-dev-ttyLF1-in-Linux-A-Core-With-BSP41-0/m-p/1891504#M7285</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;These can help:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/How-to-use-UART2-instead-of-UART1-on-LS1043ARDB-LS1046ARDB/ta-p/1750421" target="_blank"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/How-to-use-UART2-instead-of-UART1-on-LS1043ARDB-LS1046ARDB/ta-p/1750421&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32G/How-to-USE-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1814650" target="_blank"&gt;https://community.nxp.com/t5/S32G/How-to-USE-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1814650&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jun 2024 14:57:21 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-06-20T14:57:21Z</dc:date>
    <item>
      <title>How to USE UART1 (dev/ttyLF1) in Linux (A-Core) With BSP41.0</title>
      <link>https://community.nxp.com/t5/S32G/How-to-USE-UART1-dev-ttyLF1-in-Linux-A-Core-With-BSP41-0/m-p/1890353#M7272</link>
      <description>&lt;P&gt;[ 0.559933] 401c8000.serial: ttyLF0 at MMIO 0x401c8000 (irq = 37, base_baud = 7812500) is a FSL_LINFLEX&lt;BR /&gt;[ 0.569337] printk: console [ttyLF0] enabled&lt;BR /&gt;[ 0.577987] printk: bootconsole [linflex0] disabled&lt;BR /&gt;[ 0.588188] 401cc000.serial: ttyLF1 at MMIO 0x401cc000 (irq = 38, base_baud = 7812500) is a FSL_LINFLEX&lt;BR /&gt;[ 0.598021] 402bc000.serial: ttyLF2 at MMIO 0x402bc000 (irq = 59, base_baud = 7812500) is a FSL_LINFLEX&lt;/P&gt;&lt;P&gt;root@s32g274ardb2:~# ls /dev/ttyLF*&lt;BR /&gt;/dev/ttyLF0 /dev/ttyLF1 /dev/ttyLF2&lt;/P&gt;&lt;P&gt;With the default s32g274a-rdb2.dts configuration, I see the device for UART1, but this device cannot send or receive data.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How could I use&amp;nbsp; the UART1 in Linux System?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jun 2024 11:31:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-USE-UART1-dev-ttyLF1-in-Linux-A-Core-With-BSP41-0/m-p/1890353#M7272</guid>
      <dc:creator>autoexpect</dc:creator>
      <dc:date>2024-06-19T11:31:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to USE UART1 (dev/ttyLF1) in Linux (A-Core) With BSP41.0</title>
      <link>https://community.nxp.com/t5/S32G/How-to-USE-UART1-dev-ttyLF1-in-Linux-A-Core-With-BSP41-0/m-p/1891504#M7285</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;These can help:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/How-to-use-UART2-instead-of-UART1-on-LS1043ARDB-LS1046ARDB/ta-p/1750421" target="_blank"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/How-to-use-UART2-instead-of-UART1-on-LS1043ARDB-LS1046ARDB/ta-p/1750421&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32G/How-to-USE-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1814650" target="_blank"&gt;https://community.nxp.com/t5/S32G/How-to-USE-UART1-dev-ttyLF1-in-Linux-A-Core/m-p/1814650&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 14:57:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-USE-UART1-dev-ttyLF1-in-Linux-A-Core-With-BSP41-0/m-p/1891504#M7285</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-06-20T14:57:21Z</dc:date>
    </item>
  </channel>
</rss>