<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックPFE_MAC0 description in RM</title>
    <link>https://community.nxp.com/t5/S32G/PFE-MAC0-description-in-RM/m-p/1891312#M7283</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;If compare S32G2 RM and S32G3 RM, in pfe chapter, we can see below statement is removed in S32G3.&lt;/P&gt;&lt;P&gt;"PFE_MAC0 also supports 2.5 Gbit/s SGMII. When this mode is enabled, PFE_MAC1 must be used in RGMII/RMII/MII&amp;nbsp;mode if enabled"&lt;/P&gt;&lt;P&gt;I think SGMII support in gmac0 or gmac1 is mutually exclusive.&lt;/P&gt;&lt;P&gt;But how does it fix in S32G3?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jun 2024 09:37:04 GMT</pubDate>
    <dc:creator>JasonTseng</dc:creator>
    <dc:date>2024-06-20T09:37:04Z</dc:date>
    <item>
      <title>PFE_MAC0 description in RM</title>
      <link>https://community.nxp.com/t5/S32G/PFE-MAC0-description-in-RM/m-p/1891312#M7283</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;If compare S32G2 RM and S32G3 RM, in pfe chapter, we can see below statement is removed in S32G3.&lt;/P&gt;&lt;P&gt;"PFE_MAC0 also supports 2.5 Gbit/s SGMII. When this mode is enabled, PFE_MAC1 must be used in RGMII/RMII/MII&amp;nbsp;mode if enabled"&lt;/P&gt;&lt;P&gt;I think SGMII support in gmac0 or gmac1 is mutually exclusive.&lt;/P&gt;&lt;P&gt;But how does it fix in S32G3?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 09:37:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PFE-MAC0-description-in-RM/m-p/1891312#M7283</guid>
      <dc:creator>JasonTseng</dc:creator>
      <dc:date>2024-06-20T09:37:04Z</dc:date>
    </item>
    <item>
      <title>Re: PFE_MAC0 description in RM</title>
      <link>https://community.nxp.com/t5/S32G/PFE-MAC0-description-in-RM/m-p/1893151#M7312</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233050"&gt;@JasonTseng&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;There are different microprocessors. Therefore, if the feature is not mentioned on reference manual is unsupported.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jun 2024 21:53:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PFE-MAC0-description-in-RM/m-p/1893151#M7312</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2024-06-24T21:53:03Z</dc:date>
    </item>
    <item>
      <title>Re: PFE_MAC0 description in RM</title>
      <link>https://community.nxp.com/t5/S32G/PFE-MAC0-description-in-RM/m-p/1893162#M7313</link>
      <description>&lt;P&gt;Hello Brain,&lt;/P&gt;&lt;P&gt;This is a very bad answer honestly.&lt;/P&gt;&lt;P&gt;There is no doubt that S32G3 reused some S32G2 components and software.&lt;/P&gt;&lt;P&gt;Therefore some functions/features or even debugs will also move to S32G3.&lt;/P&gt;&lt;P&gt;Anyway, let me ask this question in different way.&lt;/P&gt;&lt;P&gt;Please could you provide the instructions on how to enable both SGMII on gmac0 and gmac1 simultaneously in S32G3?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jun 2024 23:10:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PFE-MAC0-description-in-RM/m-p/1893162#M7313</guid>
      <dc:creator>JasonTseng</dc:creator>
      <dc:date>2024-06-24T23:10:42Z</dc:date>
    </item>
    <item>
      <title>Re: PFE_MAC0 description in RM</title>
      <link>https://community.nxp.com/t5/S32G/PFE-MAC0-description-in-RM/m-p/1896110#M7378</link>
      <description>&lt;P&gt;Is there any update?&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 21:11:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PFE-MAC0-description-in-RM/m-p/1896110#M7378</guid>
      <dc:creator>JasonTseng</dc:creator>
      <dc:date>2024-06-28T21:11:17Z</dc:date>
    </item>
  </channel>
</rss>