<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Nxp Goldbox Setup - CAN, ETHERNET in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1890515#M7276</link>
    <description>Its okay Chenyin, I am facing few issues, listing a few below :&lt;BR /&gt;1. For the sample LED blink example, I am able to build the example, binary and elf file is getting generated. And for flashing I dont have S32 Debug Proble. So when i am trying to flash via S32 Flash Tool, the binary is getting transferred to the board, but i dont see any LED light up on the board , so i connected external LED to PA_06 , and for the blinking code also, the LED is getting ON and its not blinking.&lt;BR /&gt;2. I am having Lauterbatch with me, so if detailed steps will be provided for flashing /debugging, it would be great</description>
    <pubDate>Wed, 19 Jun 2024 15:44:08 GMT</pubDate>
    <dc:creator>dungen_master1</dc:creator>
    <dc:date>2024-06-19T15:44:08Z</dc:date>
    <item>
      <title>Nxp Goldbox Setup - CAN, ETHERNET</title>
      <link>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1883907#M7197</link>
      <description>&lt;P&gt;I am using NXP Goldbox and I am quite new to it. I need some guidance on how to start with it. I have to perform can read and write along with can parsing on the goldbox and enable ethernet port for communication.&lt;/P&gt;&lt;P&gt;Requesting kind help in this regards&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 08 Jun 2024 05:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1883907#M7197</guid>
      <dc:creator>dungen_master1</dc:creator>
      <dc:date>2024-06-08T05:20:10Z</dc:date>
    </item>
    <item>
      <title>Re: Nxp Goldbox Setup - CAN, ETHERNET</title>
      <link>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1884118#M7200</link>
      <description>&lt;P&gt;Thanks for the questions.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Firstly, you may reference the following link to get started with the board: &lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-goldbox-for-vehicle-network-processing:GS-GOLDBOX?section=out-of-the-box" target="_blank"&gt;https://www.nxp.com/document/guide/getting-started-with-the-goldbox-for-vehicle-network-processing:GS-GOLDBOX?section=out-of-the-box&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;Then reading the S32G-VNP-GLDBOX User Guide for basic board usage&lt;/LI&gt;&lt;LI&gt;Run the BSP following the BSP UM. When the board could be booted with the BSP images, the CAN/ethernet ports could be operated correctly. You may use the basic Linux commands to receive/send frames via both CAN/ethernet ports.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jun 2024 08:22:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1884118#M7200</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-06-10T08:22:00Z</dc:date>
    </item>
    <item>
      <title>Re: Nxp Goldbox Setup - CAN, ETHERNET</title>
      <link>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1885349#M7212</link>
      <description>&lt;P&gt;Can you please guide me regarding the IDE and compiler, I am getting confused with the solutions given on the website. And also if a sample code will be helpful&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jun 2024 16:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1885349#M7212</guid>
      <dc:creator>dungen_master1</dc:creator>
      <dc:date>2024-06-11T16:15:33Z</dc:date>
    </item>
    <item>
      <title>Re: Nxp Goldbox Setup - CAN, ETHERNET</title>
      <link>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1885686#M7214</link>
      <description>&lt;P&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234718"&gt;@dungen_master1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the reply.&lt;/P&gt;
&lt;P&gt;May I know your specific requirements?&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;If you want to use the CAN/ethernet on A cores with BSP, then IDE is not involved, you may only download the pre-built images and flash them to the SD to boot the board, then in Linux, you may use the CAN/ethernet directly. For samples, you may directly reference the BSP UM.&lt;/LI&gt;
&lt;LI&gt;If you want to use the CAN/ethernet on M cores, then you may have to learn to use the IDE, like S32DS and EB to generate the binaries which could be run on M cores to drive the CAN/ethernet. For samples, you may try the examples in RTD/PFE MCAL driver.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;It is a wide topic, you may try it and raise tickets for any specific issues met, we are happy to help then.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 03:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1885686#M7214</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-06-12T03:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: Nxp Goldbox Setup - CAN, ETHERNET</title>
      <link>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1888243#M7246</link>
      <description>&lt;P&gt;INTEGRATE LLCE_CAN/LIN(MCAL&amp;nbsp;DRIVER) TO S32DS 3.4 [&lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-goldbox-for-vehicle-network-processing:GS-GOLDBOX?section=integrate-llce-canlin-mcal-driver]" target="_blank"&gt;https://www.nxp.com/document/guide/getting-started-with-the-goldbox-for-vehicle-network-processing:GS-GOLDBOX?section=integrate-llce-canlin-mcal-driver]&lt;/A&gt;&amp;nbsp;I am referring this link to setup S32 Design Studio so that I can run the CAN examples given in the document. I had installed DS 3.4 and RTD, but unable to set the clock to 40 MHz and also the OS section is not coming up as shown in the screenshot&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dungen_master1_0-1718542373860.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/284338iBF8D6EDCFEC93769/image-size/medium?v=v2&amp;amp;px=400" role="button" title="dungen_master1_0-1718542373860.png" alt="dungen_master1_0-1718542373860.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;dungen_master1_0-1718542373860.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dungen_master1_1-1718542386293.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/284339i739285C652656F16/image-size/medium?v=v2&amp;amp;px=400" role="button" title="dungen_master1_1-1718542386293.png" alt="dungen_master1_1-1718542386293.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;dungen_master1_1-1718542386293.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So, if exact detailed steps would be provided, it would be really helpful&lt;/P&gt;</description>
      <pubDate>Sun, 16 Jun 2024 12:53:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1888243#M7246</guid>
      <dc:creator>dungen_master1</dc:creator>
      <dc:date>2024-06-16T12:53:37Z</dc:date>
    </item>
    <item>
      <title>Re: Nxp Goldbox Setup - CAN, ETHERNET</title>
      <link>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1890016#M7269</link>
      <description>Hi Team, can anyone please help regarding this</description>
      <pubDate>Wed, 19 Jun 2024 05:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1890016#M7269</guid>
      <dc:creator>dungen_master1</dc:creator>
      <dc:date>2024-06-19T05:00:43Z</dc:date>
    </item>
    <item>
      <title>Re: Nxp Goldbox Setup - CAN, ETHERNET</title>
      <link>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1890510#M7275</link>
      <description>&lt;P&gt;Sorry for the delay due during business trip in recent days.&lt;/P&gt;
&lt;P&gt;I noticed that my colleague has helped to start the support(via 00626886), then let’s focus on that side.&lt;/P&gt;
&lt;P&gt;Sorry for your inconvenience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jun 2024 15:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1890510#M7275</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-06-19T15:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: Nxp Goldbox Setup - CAN, ETHERNET</title>
      <link>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1890515#M7276</link>
      <description>Its okay Chenyin, I am facing few issues, listing a few below :&lt;BR /&gt;1. For the sample LED blink example, I am able to build the example, binary and elf file is getting generated. And for flashing I dont have S32 Debug Proble. So when i am trying to flash via S32 Flash Tool, the binary is getting transferred to the board, but i dont see any LED light up on the board , so i connected external LED to PA_06 , and for the blinking code also, the LED is getting ON and its not blinking.&lt;BR /&gt;2. I am having Lauterbatch with me, so if detailed steps will be provided for flashing /debugging, it would be great</description>
      <pubDate>Wed, 19 Jun 2024 15:44:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Nxp-Goldbox-Setup-CAN-ETHERNET/m-p/1890515#M7276</guid>
      <dc:creator>dungen_master1</dc:creator>
      <dc:date>2024-06-19T15:44:08Z</dc:date>
    </item>
  </channel>
</rss>