<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Qdiscs support in Linux on RDB3 hardware</title>
    <link>https://community.nxp.com/t5/S32G/Qdiscs-support-in-Linux-on-RDB3-hardware/m-p/1885142#M7209</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We are using RDB3, to configure and use TSN using GMAC interface.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Taprio (IEE 801.Qbv) can be configured in GMAC controller on hardware level.&lt;/LI&gt;&lt;LI&gt;Do we still need Taprio qdisc, to do similar thing on SW.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question is, if 801.Qbv role is done by qdisc in S/W, what is the role of ethernet controller here ?&lt;/P&gt;&lt;P&gt;if both are used what is the work offloaded to SW in comparison to HW ?&lt;/P&gt;</description>
    <pubDate>Tue, 11 Jun 2024 11:17:17 GMT</pubDate>
    <dc:creator>yellapu_anishkh</dc:creator>
    <dc:date>2024-06-11T11:17:17Z</dc:date>
    <item>
      <title>Qdiscs support in Linux on RDB3 hardware</title>
      <link>https://community.nxp.com/t5/S32G/Qdiscs-support-in-Linux-on-RDB3-hardware/m-p/1885142#M7209</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We are using RDB3, to configure and use TSN using GMAC interface.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Taprio (IEE 801.Qbv) can be configured in GMAC controller on hardware level.&lt;/LI&gt;&lt;LI&gt;Do we still need Taprio qdisc, to do similar thing on SW.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question is, if 801.Qbv role is done by qdisc in S/W, what is the role of ethernet controller here ?&lt;/P&gt;&lt;P&gt;if both are used what is the work offloaded to SW in comparison to HW ?&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jun 2024 11:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Qdiscs-support-in-Linux-on-RDB3-hardware/m-p/1885142#M7209</guid>
      <dc:creator>yellapu_anishkh</dc:creator>
      <dc:date>2024-06-11T11:17:17Z</dc:date>
    </item>
  </channel>
</rss>