<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックIPCF version on S32G2</title>
    <link>https://community.nxp.com/t5/S32G/IPCF-version-on-S32G2/m-p/1885018#M7208</link>
    <description>&lt;P&gt;I have a question.Where can I download IPCF example code for M7 on S32G274ardb2 and if I use&amp;nbsp;SW32G_RTD_4.4_4.0.2_D2306 how should I choose IPCF version?Thanks.&lt;/P&gt;</description>
    <pubDate>Tue, 11 Jun 2024 09:21:53 GMT</pubDate>
    <dc:creator>piaochunri</dc:creator>
    <dc:date>2024-06-11T09:21:53Z</dc:date>
    <item>
      <title>IPCF version on S32G2</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-version-on-S32G2/m-p/1885018#M7208</link>
      <description>&lt;P&gt;I have a question.Where can I download IPCF example code for M7 on S32G274ardb2 and if I use&amp;nbsp;SW32G_RTD_4.4_4.0.2_D2306 how should I choose IPCF version?Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jun 2024 09:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-version-on-S32G2/m-p/1885018#M7208</guid>
      <dc:creator>piaochunri</dc:creator>
      <dc:date>2024-06-11T09:21:53Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF version on S32G2</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-version-on-S32G2/m-p/1885258#M7211</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For what it is shown under the Automotive Software Package Manager, RTD v4.0.2 is being bundled with IPCF v4.9.0:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DanielAguirre_0-1718116065086.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/283508iCCC6AFA3F07CB012/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DanielAguirre_0-1718116065086.png" alt="DanielAguirre_0-1718116065086.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;We can recommend following the below steps, to create the required bundle:&lt;/P&gt;
&lt;P&gt;- Access the Automotive Software Package Manager available under the Software section of the S32G2 product page (link:&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32g-vehicle-network-processors/s32g2-processors-for-vehicle-networking:S32G2" target="_blank"&gt;S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors&lt;/A&gt;)&lt;BR /&gt;- In there, select under Devices the S32G2 option.&lt;BR /&gt;- Once selected, 3 options should be displayed: GoldVIP, Integrated Software Bundle and Integration Reference Examples. Select the Integrated Software Bundle option.&lt;BR /&gt;- Once selected, click the Generate Bundle Installer button. &lt;BR /&gt;- This action will require NXP approval for generation of the bundle. Can take up-to 48 hours to be approved. This should be noticed under the email linked to the NXP account.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jun 2024 14:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-version-on-S32G2/m-p/1885258#M7211</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-06-11T14:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF version on S32G2</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-version-on-S32G2/m-p/1885645#M7213</link>
      <description>&lt;P&gt;I have try your solution and I can not build the image because I can not find some files.What should I do?It seems that the project can not be used directly.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="piaochunri_0-1718159788890.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/283589iB31B093334707B23/image-size/medium?v=v2&amp;amp;px=400" role="button" title="piaochunri_0-1718159788890.png" alt="piaochunri_0-1718159788890.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 02:36:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-version-on-S32G2/m-p/1885645#M7213</guid>
      <dc:creator>piaochunri</dc:creator>
      <dc:date>2024-06-12T02:36:58Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF version on S32G2</title>
      <link>https://community.nxp.com/t5/S32G/IPCF-version-on-S32G2/m-p/1886224#M7224</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the capture being shared, it seems that you did not generate the code under&amp;nbsp;&lt;EM&gt;Config Tools.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;This information should be provided under the "description.txt" file under the project, if available. A similar situation is shown under the following thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32G/S32G-Use-Case-Project-FreeRTOS-Compilation-Error/td-p/1564898" target="_blank"&gt;Solved: S32G Use Case Project FreeRTOS Compilation Error - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In which, an answer was provided.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 14:12:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IPCF-version-on-S32G2/m-p/1886224#M7224</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-06-12T14:12:42Z</dc:date>
    </item>
  </channel>
</rss>