<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: HardFault_Handler</title>
    <link>https://community.nxp.com/t5/S32G/HardFault-Handler/m-p/1884608#M7206</link>
    <description>&lt;P&gt;Hello,The problem I encountered was that the pointer was pointing wrong in the program. The LLCE memory segment in my program was not initialized, and after the pointer pointed, it caused a HARD_FAULT. I hope this helps,TK.&lt;/P&gt;</description>
    <pubDate>Tue, 11 Jun 2024 02:02:07 GMT</pubDate>
    <dc:creator>peko</dc:creator>
    <dc:date>2024-06-11T02:02:07Z</dc:date>
    <item>
      <title>HardFault_Handler</title>
      <link>https://community.nxp.com/t5/S32G/HardFault-Handler/m-p/1815144#M6026</link>
      <description>&lt;P&gt;&lt;SPAN&gt;hello,&lt;/SPAN&gt;&lt;SPAN&gt;I encountered the following problem when debugging the S32G LLCE function: I have two projects, one generated by EB configuration and one generated by S32DS configuration. The program generated by EB runs to the code "u64MemPointer = (uint64*)Llce_CoreData[i].pu8MemLocation;" this code automatically jumps to the HardFault_Handler dead loop; but I tried the project generated by S32DS and there was no such phenomenon. What could be the problem? The following are screenshots of the debugging process of the two projects.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 03:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/HardFault-Handler/m-p/1815144#M6026</guid>
      <dc:creator>peko</dc:creator>
      <dc:date>2024-02-26T03:31:47Z</dc:date>
    </item>
    <item>
      <title>Re: HardFault_Handler</title>
      <link>https://community.nxp.com/t5/S32G/HardFault-Handler/m-p/1815667#M6040</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Can you let us know which S32DS/RTD/LLCE version are you working with? Are you using any NXP reference board? Also, which debugger are you using?&lt;/P&gt;
&lt;P&gt;On regards of the EB project, we might be misunderstanding it, but we don't see any example that uses that name, is this a modified project?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 14:36:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/HardFault-Handler/m-p/1815667#M6040</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-02-26T14:36:25Z</dc:date>
    </item>
    <item>
      <title>Re: HardFault_Handler</title>
      <link>https://community.nxp.com/t5/S32G/HardFault-Handler/m-p/1884333#M7204</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228204"&gt;@peko&lt;/a&gt;&amp;nbsp;Have you had any luck with this? I have the same problem, what is the solution?&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jun 2024 15:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/HardFault-Handler/m-p/1884333#M7204</guid>
      <dc:creator>Djuric</dc:creator>
      <dc:date>2024-06-10T15:33:50Z</dc:date>
    </item>
    <item>
      <title>Re: HardFault_Handler</title>
      <link>https://community.nxp.com/t5/S32G/HardFault-Handler/m-p/1884608#M7206</link>
      <description>&lt;P&gt;Hello,The problem I encountered was that the pointer was pointing wrong in the program. The LLCE memory segment in my program was not initialized, and after the pointer pointed, it caused a HARD_FAULT. I hope this helps,TK.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jun 2024 02:02:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/HardFault-Handler/m-p/1884608#M7206</guid>
      <dc:creator>peko</dc:creator>
      <dc:date>2024-06-11T02:02:07Z</dc:date>
    </item>
  </channel>
</rss>