<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Register MC EDAC with Linux EDAC subsystem in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Register-MC-EDAC-with-Linux-EDAC-subsystem/m-p/1874949#M7021</link>
    <description>&lt;P&gt;Is it because this board used inline dram which means the scrubber is obfuscating the results from the MC so the ARMs just dont have access to this information?&lt;/P&gt;</description>
    <pubDate>Sat, 25 May 2024 00:22:46 GMT</pubDate>
    <dc:creator>minersrevolt</dc:creator>
    <dc:date>2024-05-25T00:22:46Z</dc:date>
    <item>
      <title>Register MC EDAC with Linux EDAC subsystem</title>
      <link>https://community.nxp.com/t5/S32G/Register-MC-EDAC-with-Linux-EDAC-subsystem/m-p/1874807#M7020</link>
      <description>&lt;P&gt;I have an&amp;nbsp;&lt;SPAN&gt;S32G-VNP-EVB3 board running Linux using the NXP provided BSP 40. I have enabled the EDAC system in the Linux kernel to montior sbes and dbes however I do not see it in the filesystem. Makes me wonder if EDAC is actually enabled on this board? The amount of available memory seems to indicate that it is; though I could not find the memory node in the device tree to double check. Any way for me to be sure?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Expect to see edac information here,&lt;/SPAN&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/sys/devices/system/edac/mc # ls
power      subsystem  uevent&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;System memory,&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/sys/devices/system/edac/mc # cat /proc/meminfo 
MemTotal:        3500312 kB
MemFree:         3442776 kB
MemAvailable:    3442020 kB
Buffers:            1724 kB
Cached:             9168 kB
SwapCached:            0 kB
Active:             7532 kB
Inactive:           3924 kB
Active(anon):         64 kB
Inactive(anon):      640 kB
Active(file):       7468 kB
Inactive(file):     3284 kB
Unevictable:           0 kB
Mlocked:               0 kB
SwapTotal:             0 kB
SwapFree:              0 kB
Dirty:                24 kB
Writeback:             0 kB
AnonPages:           724 kB
Mapped:             2116 kB
Shmem:                60 kB
KReclaimable:      25168 kB
Slab:              33908 kB
SReclaimable:      25168 kB
SUnreclaim:         8740 kB
KernelStack:        1376 kB
PageTables:          192 kB
NFS_Unstable:          0 kB
Bounce:                0 kB
WritebackTmp:          0 kB
CommitLimit:     1750156 kB
Committed_AS:       2520 kB
VmallocTotal:   259653632 kB
VmallocUsed:        1872 kB
VmallocChunk:          0 kB
Percpu:              656 kB
CmaTotal:         262144 kB
CmaFree:          260576 kB
HugePages_Total:       0
HugePages_Free:        0
HugePages_Rsvd:        0
HugePages_Surp:        0
Hugepagesize:       2048 kB
Hugetlb:               0 kB&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 May 2024 17:05:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Register-MC-EDAC-with-Linux-EDAC-subsystem/m-p/1874807#M7020</guid>
      <dc:creator>minersrevolt</dc:creator>
      <dc:date>2024-05-24T17:05:26Z</dc:date>
    </item>
    <item>
      <title>Re: Register MC EDAC with Linux EDAC subsystem</title>
      <link>https://community.nxp.com/t5/S32G/Register-MC-EDAC-with-Linux-EDAC-subsystem/m-p/1874949#M7021</link>
      <description>&lt;P&gt;Is it because this board used inline dram which means the scrubber is obfuscating the results from the MC so the ARMs just dont have access to this information?&lt;/P&gt;</description>
      <pubDate>Sat, 25 May 2024 00:22:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Register-MC-EDAC-with-Linux-EDAC-subsystem/m-p/1874949#M7021</guid>
      <dc:creator>minersrevolt</dc:creator>
      <dc:date>2024-05-25T00:22:46Z</dc:date>
    </item>
    <item>
      <title>Re: Register MC EDAC with Linux EDAC subsystem</title>
      <link>https://community.nxp.com/t5/S32G/Register-MC-EDAC-with-Linux-EDAC-subsystem/m-p/1875835#M7041</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234092" target="_blank"&gt;minersrevolt&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;From BSP perspective, it does not support EDAC at DDR level.&lt;/P&gt;
&lt;P&gt;Sorry for your inconvenience.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 02:36:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Register-MC-EDAC-with-Linux-EDAC-subsystem/m-p/1875835#M7041</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-05-28T02:36:38Z</dc:date>
    </item>
  </channel>
</rss>