<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Bootloader start M core and A53 Linux at the same time</title>
    <link>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1870839#M6995</link>
    <description>&lt;P&gt;I referred to the document "32G Bootloader Customization V2" to create the bootloader for S32g274a, but I encountered some problems. The bootloader can boot A53core into Linux independently and can also boot the llce CAN-Loopback program on M7core separately. However, when booting the llce CAN-Loopback program on both A53 and M7 simultaneously, A53core gets stuck in Linux and cannot enter rootfs, and the M7 program cannot run properly. But when I blocked the Platform-Init (null) function in the M7 program, I was able to enter Linux normally. I think the interrupt in the llce CAN_loopback program affected it，Can you help me modify this interrupt conflict？&lt;/P&gt;</description>
    <pubDate>Wed, 22 May 2024 14:13:08 GMT</pubDate>
    <dc:creator>LB666</dc:creator>
    <dc:date>2024-05-22T14:13:08Z</dc:date>
    <item>
      <title>Bootloader start M core and A53 Linux at the same time</title>
      <link>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1870839#M6995</link>
      <description>&lt;P&gt;I referred to the document "32G Bootloader Customization V2" to create the bootloader for S32g274a, but I encountered some problems. The bootloader can boot A53core into Linux independently and can also boot the llce CAN-Loopback program on M7core separately. However, when booting the llce CAN-Loopback program on both A53 and M7 simultaneously, A53core gets stuck in Linux and cannot enter rootfs, and the M7 program cannot run properly. But when I blocked the Platform-Init (null) function in the M7 program, I was able to enter Linux normally. I think the interrupt in the llce CAN_loopback program affected it，Can you help me modify this interrupt conflict？&lt;/P&gt;</description>
      <pubDate>Wed, 22 May 2024 14:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1870839#M6995</guid>
      <dc:creator>LB666</dc:creator>
      <dc:date>2024-05-22T14:13:08Z</dc:date>
    </item>
    <item>
      <title>回复： Bootloader start M core and A53 Linux at the same time</title>
      <link>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1871421#M7002</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24888"&gt;@Johnli&lt;/a&gt;&amp;nbsp;&amp;nbsp;Can you give me some help? Thank you&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 01:22:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1871421#M7002</guid>
      <dc:creator>LB666</dc:creator>
      <dc:date>2024-05-23T01:22:11Z</dc:date>
    </item>
    <item>
      <title>回复： Bootloader start M core and A53 Linux at the same time</title>
      <link>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1871434#M7003</link>
      <description>&lt;P&gt;pls check:&lt;/P&gt;&lt;TABLE width="1110"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="271"&gt;S32G_Bootloader_G3_LLCELOGGER&lt;/TD&gt;&lt;TD width="154"&gt;doc&amp;amp;project explain the G3 bootloader customizaiton(similar with G2) to run logger demo&lt;/TD&gt;&lt;TD width="685"&gt;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-Bootloader-G3-Customization/ta-p/1769528" target="_blank"&gt;https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-Bootloader-G3-Customization/ta-p/1769528&lt;/A&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 01:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1871434#M7003</guid>
      <dc:creator>Johnli</dc:creator>
      <dc:date>2024-05-23T01:39:00Z</dc:date>
    </item>
    <item>
      <title>回复： Bootloader start M core and A53 Linux at the same time</title>
      <link>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1871467#M7004</link>
      <description>&lt;P&gt;I have reviewed this document, but still encountered the above issue. I am running the llce can'loopback program on the M7 core. I would like to confirm that my bootloader can successfully boot Linux separately. Does this mean that the clock in my bootloader and ATF is configured correctly? I hope you can help me analyze the above issues.Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 02:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1871467#M7004</guid>
      <dc:creator>LB666</dc:creator>
      <dc:date>2024-05-23T02:13:46Z</dc:date>
    </item>
    <item>
      <title>回复： Bootloader start M core and A53 Linux at the same time</title>
      <link>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1871474#M7005</link>
      <description>&lt;P&gt;run the demo directly, which on the link.&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 02:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1871474#M7005</guid>
      <dc:creator>Johnli</dc:creator>
      <dc:date>2024-05-23T02:19:38Z</dc:date>
    </item>
    <item>
      <title>回复： Bootloader start M core and A53 Linux at the same time</title>
      <link>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1871485#M7006</link>
      <description>We are using the s32g274A chip and have not purchased the LLce Logger</description>
      <pubDate>Thu, 23 May 2024 02:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Bootloader-start-M-core-and-A53-Linux-at-the-same-time/m-p/1871485#M7006</guid>
      <dc:creator>LB666</dc:creator>
      <dc:date>2024-05-23T02:31:30Z</dc:date>
    </item>
  </channel>
</rss>