<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G2  Linux BSP build fail in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G2-Linux-BSP-build-fail/m-p/1866064#M6906</link>
    <description>&lt;P&gt;From the BSP39.0 UM, it is mentioned that &amp;nbsp;&lt;/P&gt;
&lt;P&gt;“All the steps described below have been run and validated on Ubuntu-20.04 LTS (native or through a virtual machine). It is then recommended to install Ubuntu-20.04 LTS before going through the following sections.”&lt;/P&gt;
&lt;P&gt;“A Yocto build needs at least 50GB of free space and takes a lot of time (2 to 10 hours, depending on the system configuration). It is recommended to use a powerful system with many cores and a fast storage media (SSD is recommended). The recommended RAM size is 8 GB.”&lt;/P&gt;
&lt;P&gt;So, in summary, it is suggested that:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Host: Ubuntu20.04-LTS is recommended.&lt;/LI&gt;
&lt;LI&gt;DDR: 8GB+ is recommended.&lt;/LI&gt;
&lt;LI&gt;Storage: SSD is recommended, better to have large size&lt;/LI&gt;
&lt;LI&gt;CPU: Powerful CPU with many cores.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 15 May 2024 07:55:26 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2024-05-15T07:55:26Z</dc:date>
    <item>
      <title>S32G2  Linux BSP build fail</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Linux-BSP-build-fail/m-p/1865130#M6884</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; I chose YOCTO to build Linux-BSP 39.0, I chose to build auto target&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;my ubuntu is 22.04, 8 cores and memory more than 8M, is it OK?&amp;nbsp; (Ubuntu version must be 18.04.4 LTS?)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; My PC restarts everytime and build failed.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;SPAN&gt;What are the minimum requirements for the number of cores, memory, and operating system for the compiler PC?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 07:54:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Linux-BSP-build-fail/m-p/1865130#M6884</guid>
      <dc:creator>yangjinzhuang</dc:creator>
      <dc:date>2024-05-14T07:54:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2  Linux BSP build fail</title>
      <link>https://community.nxp.com/t5/S32G/S32G2-Linux-BSP-build-fail/m-p/1866064#M6906</link>
      <description>&lt;P&gt;From the BSP39.0 UM, it is mentioned that &amp;nbsp;&lt;/P&gt;
&lt;P&gt;“All the steps described below have been run and validated on Ubuntu-20.04 LTS (native or through a virtual machine). It is then recommended to install Ubuntu-20.04 LTS before going through the following sections.”&lt;/P&gt;
&lt;P&gt;“A Yocto build needs at least 50GB of free space and takes a lot of time (2 to 10 hours, depending on the system configuration). It is recommended to use a powerful system with many cores and a fast storage media (SSD is recommended). The recommended RAM size is 8 GB.”&lt;/P&gt;
&lt;P&gt;So, in summary, it is suggested that:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Host: Ubuntu20.04-LTS is recommended.&lt;/LI&gt;
&lt;LI&gt;DDR: 8GB+ is recommended.&lt;/LI&gt;
&lt;LI&gt;Storage: SSD is recommended, better to have large size&lt;/LI&gt;
&lt;LI&gt;CPU: Powerful CPU with many cores.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 May 2024 07:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G2-Linux-BSP-build-fail/m-p/1866064#M6906</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-05-15T07:55:26Z</dc:date>
    </item>
  </channel>
</rss>