<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: LLCE LIN in Linux</title>
    <link>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1856202#M6735</link>
    <description>Hello Chen,&lt;BR /&gt;This driver under Linux, can only be used as uart mode. If I want to use the LIN protocol to transmit, is it not supported?&lt;BR /&gt;</description>
    <pubDate>Sun, 28 Apr 2024 08:11:19 GMT</pubDate>
    <dc:creator>Alex_mjl</dc:creator>
    <dc:date>2024-04-28T08:11:19Z</dc:date>
    <item>
      <title>LLCE LIN in Linux</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1855349#M6725</link>
      <description>&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Refer to the S32G_Linux BSP38 documentation,&amp;nbsp;It seems that LLCE LIN is already supported in Linux. As show below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alex_mjl_0-1714110935715.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/276045i8409F6D85271AB70/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alex_mjl_0-1714110935715.png" alt="Alex_mjl_0-1714110935715.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;I want to know how to use LLCE LIN in Linux?&lt;/P&gt;</description>
      <pubDate>Fri, 26 Apr 2024 05:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1855349#M6725</guid>
      <dc:creator>Alex_mjl</dc:creator>
      <dc:date>2024-04-26T05:56:57Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE LIN in Linux</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1856182#M6733</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224758" target="_blank"&gt;Alex_mjl&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks for the question.&lt;/P&gt;&lt;P&gt;Yes, it could be used in UART mode, the kernel could be compiled as listed in the BSP UM, but one important limitation is that LLCE LINFlexD can be used as a serial console once the LLCE mailbox driver has been loaded, typically after reaching the Linux console.&lt;/P&gt;&lt;P&gt;However, by default, the serial driver is loaded before loading the LLCE modules, so that only LINFlexD consoles are enabled during the boot. You may have to make some modification to the system to insure the driver loading order to have the LLCELIN correctly probed by the driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Chenyin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 28 Apr 2024 07:36:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1856182#M6733</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-04-28T07:36:37Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE LIN in Linux</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1856202#M6735</link>
      <description>Hello Chen,&lt;BR /&gt;This driver under Linux, can only be used as uart mode. If I want to use the LIN protocol to transmit, is it not supported?&lt;BR /&gt;</description>
      <pubDate>Sun, 28 Apr 2024 08:11:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1856202#M6735</guid>
      <dc:creator>Alex_mjl</dc:creator>
      <dc:date>2024-04-28T08:11:19Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE LIN in Linux</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1857124#M6750</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224758" target="_blank" rel="noopener"&gt;Alex_mjl&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks for the feedback.&lt;/P&gt;&lt;P&gt;As indicated in the BSP UM, only UART mode is supported for LINFlexD based on Linux BSP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Chenyin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Apr 2024 02:17:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1857124#M6750</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-04-30T02:17:05Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE LIN in Linux</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1857128#M6751</link>
      <description>Thank you for your answer.</description>
      <pubDate>Tue, 30 Apr 2024 02:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-LIN-in-Linux/m-p/1857128#M6751</guid>
      <dc:creator>Alex_mjl</dc:creator>
      <dc:date>2024-04-30T02:21:51Z</dc:date>
    </item>
  </channel>
</rss>