<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LLCE Linux S32G in S32G</title>
    <link>https://community.nxp.com/t5/S32G/LLCE-Linux-S32G/m-p/1844719#M6619</link>
    <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229803" target="_blank"&gt;Abhiram_m_s&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks for the question, would you please help to clarify the following?&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;May I know if you are using the custom board or RDB? It is based on S32G2 or G3?&lt;/LI&gt;&lt;LI&gt;May I know which example/demo you are testing with?&lt;/LI&gt;&lt;LI&gt;What is the modification to the conf/local.conf, would you please help to provide the steps you have done?&lt;/LI&gt;&lt;LI&gt;From the logs, seems it is a ubuntu RFS, then you have done a ubuntu build based on BSP38.0 using yocto?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Chenyin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 11 Apr 2024 03:04:32 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2024-04-11T03:04:32Z</dc:date>
    <item>
      <title>LLCE Linux S32G</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-Linux-S32G/m-p/1843700#M6612</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I am trying to solve LLCE can using Linux. I am facing few issues.&lt;/P&gt;&lt;P&gt;After editing local.conf file and after compiling the linux kernel, i am not able to configure CAN&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Abhiram_m_s_0-1712733710734.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/272866i3E429660D23C1206/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Abhiram_m_s_0-1712733710734.png" alt="Abhiram_m_s_0-1712733710734.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Can you let me know how to proceed and also if possible, can you give me the clear steps for this demo.&lt;/P&gt;&lt;P&gt;I am using LLCE 1.0.7 and RTD 4.0.2 and linux BSP 38.0&lt;/P&gt;&lt;P&gt;Thank you. Regards.&lt;BR /&gt;Abhiram M S&lt;/P&gt;</description>
      <pubDate>Wed, 10 Apr 2024 07:22:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-Linux-S32G/m-p/1843700#M6612</guid>
      <dc:creator>Abhiram_m_s</dc:creator>
      <dc:date>2024-04-10T07:22:56Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE Linux S32G</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-Linux-S32G/m-p/1844719#M6619</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229803" target="_blank"&gt;Abhiram_m_s&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks for the question, would you please help to clarify the following?&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;May I know if you are using the custom board or RDB? It is based on S32G2 or G3?&lt;/LI&gt;&lt;LI&gt;May I know which example/demo you are testing with?&lt;/LI&gt;&lt;LI&gt;What is the modification to the conf/local.conf, would you please help to provide the steps you have done?&lt;/LI&gt;&lt;LI&gt;From the logs, seems it is a ubuntu RFS, then you have done a ubuntu build based on BSP38.0 using yocto?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Chenyin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Apr 2024 03:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-Linux-S32G/m-p/1844719#M6619</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-04-11T03:04:32Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE Linux S32G</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-Linux-S32G/m-p/1844741#M6620</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24163"&gt;@chenyin_h&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;We are using S32G3-VNP-RDB3 board.&lt;/LI&gt;&lt;LI&gt;We are trying to execute LLCE can demo&lt;/LI&gt;&lt;LI&gt;We have added the following 2 lines for the local.conf file&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN&gt;DISTRO_FEATURES_append = " llce-can "&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP_FIRMWARE_LOCAL_DIR = "/path/to/firmware/binaries/folder"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4. We have done ubuntu build based on BSP 38.0 using yocto.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Apr 2024 03:35:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-Linux-S32G/m-p/1844741#M6620</guid>
      <dc:creator>Abhiram_m_s</dc:creator>
      <dc:date>2024-04-11T03:35:10Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE Linux S32G</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-Linux-S32G/m-p/1847112#M6651</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229803" target="_blank"&gt;Abhiram_m_s&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks for the feedback.&lt;/P&gt;
&lt;P&gt;I will have a test with Yocto to see if there are issues, would you please compiling the kernel/modules manually to have a try?&lt;/P&gt;
&lt;P&gt;I could confirm that it works fine with LLCECAN interface on BSP38.0, the reference steps are shown below:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Add the following configuration to the kernel config&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;_Networking support&lt;/P&gt;
&lt;P&gt;_CAN bus subsystem support&lt;/P&gt;
&lt;P&gt;_CAN Device Drivers&lt;/P&gt;
&lt;P&gt;_Platform CAN drivers with Netlink support&lt;/P&gt;
&lt;P&gt;_NXP LLCE CAN Support&lt;/P&gt;
&lt;P&gt;&amp;lt;M&amp;gt;&amp;nbsp;&amp;nbsp; LLCE CAN&lt;/P&gt;
&lt;OL start="2"&gt;
&lt;LI&gt;Build the kernel/modules, copy kernel image, ./drivers/net/can/llce/llce_can.ko, ./drivers/mailbox/llce-mailbox.ko ./drivers/mfd/llce-core.ko to the SD card.&lt;/LI&gt;
&lt;LI&gt;Copy the LLCE firmware binaries to the /lib/firmware on the SD card, including dte.bin, frpe.bin, ppe_tx.bin, ppe_rx.bin.&lt;/LI&gt;
&lt;LI&gt;Boot the board with newly built kernel image on the SD card&lt;/LI&gt;
&lt;LI&gt;Insmod the three modules following the order with: &amp;nbsp;llce-core.ko, llce-mailbox.ko, llce_can.ko&lt;/LI&gt;
&lt;LI&gt;Setup the llcecan port by the following commands:&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;ip link set up llcecan0 type can bitrate 500000 dbitrate 5000000 fd on&lt;/P&gt;
&lt;P&gt;ip link set up llcecan14 type can bitrate 500000 dbitrate 5000000 fd on&lt;/P&gt;
&lt;OL start="7"&gt;
&lt;LI&gt;Connect the llcecan0 and llcecan14 to have a test with candump/cansend.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 12:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-Linux-S32G/m-p/1847112#M6651</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-04-15T12:00:46Z</dc:date>
    </item>
  </channel>
</rss>