<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: Downloading OS for SD Card - NXP Goldbox</title>
    <link>https://community.nxp.com/t5/S32G/Downloading-OS-for-SD-Card-NXP-Goldbox/m-p/1840289#M6539</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This image should be available under the Automotive Software Package Manager inside the S32G3 product page (link:&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32g-vehicle-network-processors/s32g3-processors-for-vehicle-networking:S32G3" target="_blank"&gt;S32G3 Safe and Secure Vehicle Network Processor | NXP Semiconductors&lt;/A&gt;). Once under the&amp;nbsp;&lt;EM&gt;Automotive Software Package Manager&lt;/EM&gt;, there is a bundle dedicated to GoldVIP, in which all binaries are provided.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Wed, 03 Apr 2024 18:18:49 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2024-04-03T18:18:49Z</dc:date>
    <item>
      <title>Downloading OS for SD Card - NXP Goldbox</title>
      <link>https://community.nxp.com/t5/S32G/Downloading-OS-for-SD-Card-NXP-Goldbox/m-p/1840208#M6535</link>
      <description>&lt;P&gt;I have to flash a new SD Card with the orignal image of NXP Goldbox, so requesting for the download link&lt;/P&gt;</description>
      <pubDate>Wed, 03 Apr 2024 15:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Downloading-OS-for-SD-Card-NXP-Goldbox/m-p/1840208#M6535</guid>
      <dc:creator>dungen_master</dc:creator>
      <dc:date>2024-04-03T15:21:23Z</dc:date>
    </item>
    <item>
      <title>Re: Downloading OS for SD Card - NXP Goldbox</title>
      <link>https://community.nxp.com/t5/S32G/Downloading-OS-for-SD-Card-NXP-Goldbox/m-p/1840289#M6539</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This image should be available under the Automotive Software Package Manager inside the S32G3 product page (link:&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32g-vehicle-network-processors/s32g3-processors-for-vehicle-networking:S32G3" target="_blank"&gt;S32G3 Safe and Secure Vehicle Network Processor | NXP Semiconductors&lt;/A&gt;). Once under the&amp;nbsp;&lt;EM&gt;Automotive Software Package Manager&lt;/EM&gt;, there is a bundle dedicated to GoldVIP, in which all binaries are provided.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Apr 2024 18:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Downloading-OS-for-SD-Card-NXP-Goldbox/m-p/1840289#M6539</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-04-03T18:18:49Z</dc:date>
    </item>
  </channel>
</rss>