<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32DS flash programming with Script language</title>
    <link>https://community.nxp.com/t5/S32G/S32DS-flash-programming-with-Script-language/m-p/1838964#M6505</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We want to automatize a process with scripting languages, not by opening S32DS, but with a .bat file or something similar. However, we don't know where to start. The thing is that we wrote a code that programs OTP once executing in RAM mode. The second stage will be programming the flash with a xxx.bin file.&lt;/P&gt;&lt;P&gt;How can we achieve this? Can we use tcl scripting or Is there any other way?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Apr 2024 05:58:46 GMT</pubDate>
    <dc:creator>Fergani</dc:creator>
    <dc:date>2024-04-02T05:58:46Z</dc:date>
    <item>
      <title>S32DS flash programming with Script language</title>
      <link>https://community.nxp.com/t5/S32G/S32DS-flash-programming-with-Script-language/m-p/1838964#M6505</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We want to automatize a process with scripting languages, not by opening S32DS, but with a .bat file or something similar. However, we don't know where to start. The thing is that we wrote a code that programs OTP once executing in RAM mode. The second stage will be programming the flash with a xxx.bin file.&lt;/P&gt;&lt;P&gt;How can we achieve this? Can we use tcl scripting or Is there any other way?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 05:58:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32DS-flash-programming-with-Script-language/m-p/1838964#M6505</guid>
      <dc:creator>Fergani</dc:creator>
      <dc:date>2024-04-02T05:58:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS flash programming with Script language</title>
      <link>https://community.nxp.com/t5/S32G/S32DS-flash-programming-with-Script-language/m-p/1839462#M6521</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the available information, this does not seem to be a flow that NXP has documentation on, the expectation is the usage of either S32DS IDE or a different Configuration tool. We see the following HOWTO is available under the S32DS community:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Command-Line-Interface/ta-p/1112410" target="_blank"&gt;HOWTO: S32 Design Studio Command Line Interface - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In which it is shown that under the "Help &amp;gt; Help Contents":&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DanielAguirre_0-1712068434708.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/271592i8AE4EE4C32DDAD68/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DanielAguirre_0-1712068434708.png" alt="DanielAguirre_0-1712068434708.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;CLI information will be provided.&lt;/P&gt;
&lt;P&gt;Aside from this, not much more is provided. We do apologize.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 14:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32DS-flash-programming-with-Script-language/m-p/1839462#M6521</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-04-02T14:34:41Z</dc:date>
    </item>
  </channel>
</rss>