<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックLLCE Interrupt latency</title>
    <link>https://community.nxp.com/t5/S32G/LLCE-Interrupt-latency/m-p/1836010#M6415</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are using all the four LLCE LINFLEXD channels as UART with LLCE interrupt forwarding in our s32g2 rev2 system.&lt;/P&gt;&lt;P&gt;in Linflexd, FOR UART we have enabled the RX interrupts.&lt;/P&gt;&lt;P&gt;Here RX interrutpts are always enabled, and as soon as data is received, ISR is exceuted and data is stored in a circular buffer.&lt;/P&gt;&lt;P&gt;This data is taken by application for further processing.&lt;/P&gt;&lt;P&gt;The issue we are seeing is that the interrupt latency for RX seems to be sometimes more, i.e ISR is called or executed with a higher latency period.&lt;/P&gt;&lt;P&gt;as per our previous conversations with the NXP, it was understood that the only one ISR is available for all the channles of LLCE LINFLEXD.&lt;/P&gt;&lt;P&gt;is there any way that we can reduce the interrupt latency, or is there any way to create ISR for each LINFLEXD channels, which would really improve our system performance.&lt;/P&gt;</description>
    <pubDate>Wed, 27 Mar 2024 06:16:59 GMT</pubDate>
    <dc:creator>Naveenkumar_Muthusamy</dc:creator>
    <dc:date>2024-03-27T06:16:59Z</dc:date>
    <item>
      <title>LLCE Interrupt latency</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-Interrupt-latency/m-p/1836010#M6415</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are using all the four LLCE LINFLEXD channels as UART with LLCE interrupt forwarding in our s32g2 rev2 system.&lt;/P&gt;&lt;P&gt;in Linflexd, FOR UART we have enabled the RX interrupts.&lt;/P&gt;&lt;P&gt;Here RX interrutpts are always enabled, and as soon as data is received, ISR is exceuted and data is stored in a circular buffer.&lt;/P&gt;&lt;P&gt;This data is taken by application for further processing.&lt;/P&gt;&lt;P&gt;The issue we are seeing is that the interrupt latency for RX seems to be sometimes more, i.e ISR is called or executed with a higher latency period.&lt;/P&gt;&lt;P&gt;as per our previous conversations with the NXP, it was understood that the only one ISR is available for all the channles of LLCE LINFLEXD.&lt;/P&gt;&lt;P&gt;is there any way that we can reduce the interrupt latency, or is there any way to create ISR for each LINFLEXD channels, which would really improve our system performance.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Mar 2024 06:16:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-Interrupt-latency/m-p/1836010#M6415</guid>
      <dc:creator>Naveenkumar_Muthusamy</dc:creator>
      <dc:date>2024-03-27T06:16:59Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE Interrupt latency</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-Interrupt-latency/m-p/1836970#M6446</link>
      <description>&lt;P&gt;hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205137"&gt;@Daniel-Aguirre&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;any update on this issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Mar 2024 06:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-Interrupt-latency/m-p/1836970#M6446</guid>
      <dc:creator>Naveenkumar_Muthusamy</dc:creator>
      <dc:date>2024-03-28T06:02:39Z</dc:date>
    </item>
  </channel>
</rss>