<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Debugging Linux application on S32G-VNP-RDB2 using S32G Debug Probe</title>
    <link>https://community.nxp.com/t5/S32G/Debugging-Linux-application-on-S32G-VNP-RDB2-using-S32G-Debug/m-p/1432001#M641</link>
    <description>&lt;P&gt;I am designing Linux based application using&amp;nbsp;S32G-VNP-RDB2.&lt;/P&gt;&lt;P&gt;I received board and Linux SD card. I can able to boot board and able access board over UART0 using minicom.&lt;/P&gt;&lt;P&gt;I have also purchased S32G Debug probe. Now I want to connect this probe to board and start my development using S32G Design Studio. I want to using only single A53 core in my application.&lt;/P&gt;&lt;P&gt;When I tried open debugger configuration, no any device is present (please find attached screenshot for more detail)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="prafullb_0-1647953127005.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174420i81303EA0327A946B/image-size/medium?v=v2&amp;amp;px=400" alt="prafullb_0-1647953127005.png" title="prafullb_0-1647953127005.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use S32G Design Studio and S32Debugger port to configure peripherals and develop Linux based application.?&amp;nbsp;Can anybody please guide me how to proceed now.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Additional Information :&lt;/P&gt;&lt;P&gt;Debugger drivers are installed properly and Tx/Rx LED is blinking as well as RUN/PAUSE LED is constantly glowing as RED.&lt;/P&gt;</description>
    <pubDate>Tue, 22 Mar 2022 12:53:48 GMT</pubDate>
    <dc:creator>prafull_barpute</dc:creator>
    <dc:date>2022-03-22T12:53:48Z</dc:date>
    <item>
      <title>Debugging Linux application on S32G-VNP-RDB2 using S32G Debug Probe</title>
      <link>https://community.nxp.com/t5/S32G/Debugging-Linux-application-on-S32G-VNP-RDB2-using-S32G-Debug/m-p/1432001#M641</link>
      <description>&lt;P&gt;I am designing Linux based application using&amp;nbsp;S32G-VNP-RDB2.&lt;/P&gt;&lt;P&gt;I received board and Linux SD card. I can able to boot board and able access board over UART0 using minicom.&lt;/P&gt;&lt;P&gt;I have also purchased S32G Debug probe. Now I want to connect this probe to board and start my development using S32G Design Studio. I want to using only single A53 core in my application.&lt;/P&gt;&lt;P&gt;When I tried open debugger configuration, no any device is present (please find attached screenshot for more detail)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="prafullb_0-1647953127005.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174420i81303EA0327A946B/image-size/medium?v=v2&amp;amp;px=400" alt="prafullb_0-1647953127005.png" title="prafullb_0-1647953127005.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is it possible to use S32G Design Studio and S32Debugger port to configure peripherals and develop Linux based application.?&amp;nbsp;Can anybody please guide me how to proceed now.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Additional Information :&lt;/P&gt;&lt;P&gt;Debugger drivers are installed properly and Tx/Rx LED is blinking as well as RUN/PAUSE LED is constantly glowing as RED.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Mar 2022 12:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Debugging-Linux-application-on-S32G-VNP-RDB2-using-S32G-Debug/m-p/1432001#M641</guid>
      <dc:creator>prafull_barpute</dc:creator>
      <dc:date>2022-03-22T12:53:48Z</dc:date>
    </item>
  </channel>
</rss>