<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: S32 Design Studio on Linux with S32G2 SDK - Problems</title>
    <link>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431002#M630</link>
    <description>&lt;P&gt;Where exactly do you need to change the path?&amp;nbsp; I have installed the design studio Version: 3.4&lt;BR /&gt;Build id: 201217 (Update 3) on Ubuntu 20.04, its an arduous task just to install the software, it needs around 5GB hard disk space and almost 2 hours to install.&lt;/P&gt;&lt;P&gt;After installation I have to install Oracle JDK or else it won't start.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After it started, it was again installing the SDK's which took another hour.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Can_Do_bus_0-1647829626799.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174208i664E2CCBD2D4CE07/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Can_Do_bus_0-1647829626799.png" alt="Can_Do_bus_0-1647829626799.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After this when I try to create a project from example, the examples are not there I only see these two&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Can_Do_bus_1-1647829712003.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174209iBF7E8D87BB75EE98/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Can_Do_bus_1-1647829712003.png" alt="Can_Do_bus_1-1647829712003.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The pin configuration tool also complains processor not chosen, how to fix this?&lt;/P&gt;</description>
    <pubDate>Mon, 21 Mar 2022 02:29:06 GMT</pubDate>
    <dc:creator>Can_Do_bus</dc:creator>
    <dc:date>2022-03-21T02:29:06Z</dc:date>
    <item>
      <title>S32 Design Studio on Linux with S32G2 SDK - Problems</title>
      <link>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1411772#M509</link>
      <description>&lt;P&gt;I have installed S32DS 3.4 on Ubuntu 18.04 and had some issues, and wondering if anyone else had similar problems and find any solution.&lt;/P&gt;&lt;P&gt;I have followed instructions on the S32DS_Installation_Guide_3.4.0 document and it completed and run succesfully. Then I have installed RTD and other drivers.&lt;/P&gt;&lt;P&gt;First issue is that "S32DS Extensions and Updates" window somehow do not show every package. S32G2 Development pack, GCC toolchains S32 Design Studio and Configuration Tools 3.4.1 package (comes with package manager bundle) are there, but other SDK packages did not appear after adding the update-site. I worked around this using Help/Install new software... section which let me install those packages.&lt;/P&gt;&lt;P&gt;The other issue is, although configuration tools run and seems to work fine, they do not generate &lt;STRONG&gt;some of &lt;/STRONG&gt;generated source code. I have tried FreeRTOS toggle led example and RTD Siul Dio Ip example for S32G274A, peripheral tool did not generate Suil related code (others generated fine) without showing any errors and I was unable to build.&lt;/P&gt;&lt;P&gt;I have tried several fresh installation, tried using only package manager bundle SDKs, Configuration Tools 3.4.1 and 3.4.3 versions and RTD HF2, HF4, 3.0 versions the results never changed.&lt;/P&gt;&lt;P&gt;I do not know if S32G2 SDK is officially supported for Linux, I am guessing not. However it looks like it is almost there, also seems a lot quicker and more efficient than on Windows. I am posting because maybe somebody had a workaround about second issue or NXP would know about it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Feb 2022 11:04:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1411772#M509</guid>
      <dc:creator>halilmutlu</dc:creator>
      <dc:date>2022-02-10T11:04:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio on Linux with S32G2 SDK - Problems</title>
      <link>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1413056#M519</link>
      <description>&lt;P&gt;Found the problem. The paths in the SDK files were written case-insensitively, which is OK for Windows but not for Linux. Manually changing them fixed the issue and example built correctly.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Feb 2022 11:17:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1413056#M519</guid>
      <dc:creator>halilmutlu</dc:creator>
      <dc:date>2022-02-14T11:17:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio on Linux with S32G2 SDK - Problems</title>
      <link>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431002#M630</link>
      <description>&lt;P&gt;Where exactly do you need to change the path?&amp;nbsp; I have installed the design studio Version: 3.4&lt;BR /&gt;Build id: 201217 (Update 3) on Ubuntu 20.04, its an arduous task just to install the software, it needs around 5GB hard disk space and almost 2 hours to install.&lt;/P&gt;&lt;P&gt;After installation I have to install Oracle JDK or else it won't start.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After it started, it was again installing the SDK's which took another hour.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Can_Do_bus_0-1647829626799.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174208i664E2CCBD2D4CE07/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Can_Do_bus_0-1647829626799.png" alt="Can_Do_bus_0-1647829626799.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After this when I try to create a project from example, the examples are not there I only see these two&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Can_Do_bus_1-1647829712003.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174209iBF7E8D87BB75EE98/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Can_Do_bus_1-1647829712003.png" alt="Can_Do_bus_1-1647829712003.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The pin configuration tool also complains processor not chosen, how to fix this?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 02:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431002#M630</guid>
      <dc:creator>Can_Do_bus</dc:creator>
      <dc:date>2022-03-21T02:29:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio on Linux with S32G2 SDK - Problems</title>
      <link>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431130#M633</link>
      <description>&lt;P&gt;It looks like SDK is not installed correctly, you should have seen the examples if otherwise. For first time setup, I would follow the manuals step by step and do everything on Windows (since it is the actual supported OS for the SDKs).&lt;/P&gt;&lt;P&gt;Nevertheless to answer your question what exactly I change to solve my problem,&lt;/P&gt;&lt;P&gt;under installation directory in folder "NXP/S32DS.3.4/eclipse/mcu_data/components ", there are data for generating code. These file names and their references in the .js files are written case insensitively. I have changed the ones I could catch manually, that has done the job.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 07:53:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431130#M633</guid>
      <dc:creator>halilmutlu</dc:creator>
      <dc:date>2022-03-21T07:53:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio on Linux with S32G2 SDK - Problems</title>
      <link>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431278#M634</link>
      <description>&lt;P&gt;Thank you for replying, it appears those examples are based on S32_SDK_RTM however only the Freemaster SDK is installed as the part of Design studio, can you please check whether you have the S32_SDK_RTM installed on your linux version. I have posted a separate &lt;A href="https://community.nxp.com/t5/S32-Design-Studio/S32-Design-Studio-for-S32-Platform-Version-3-4-Build-id-201217/m-p/1431088#M8356" target="_self"&gt;thread&lt;/A&gt; just to get some official response.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a separate installation of Design Studio ARM 2.2 that has the examples installed correctly which has both freemaster SDK and S32SDK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was tempted to install this monster under the assumption that it will do the pin configurations etc on Linux.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 11:44:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431278#M634</guid>
      <dc:creator>Can_Do_bus</dc:creator>
      <dc:date>2022-03-21T11:44:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio on Linux with S32G2 SDK - Problems</title>
      <link>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431289#M635</link>
      <description>&lt;P&gt;Normally SDKs are installed through Extensions &amp;amp; Updates tool addressing update-site zip files as explained &lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Offline-Install-of-Extensions-and/ta-p/1126424" target="_self"&gt;here&lt;/A&gt;. But as I mentioned in the post, in Linux, most packages do not appear (probably because they do not have official linux support) so I have installed them through "Install New Software..." section, addressing update-site zip archives. I always install and test them on Windows machine before installing on linux though.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 12:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431289#M635</guid>
      <dc:creator>halilmutlu</dc:creator>
      <dc:date>2022-03-21T12:19:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio on Linux with S32G2 SDK - Problems</title>
      <link>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431394#M636</link>
      <description>&lt;P&gt;Thanks for engaging, my issue is mainly to find those zip files, the SDK I found on NXP site was an exe and not a zip file. Do you have a link?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 15:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431394#M636</guid>
      <dc:creator>Can_Do_bus</dc:creator>
      <dc:date>2022-03-21T15:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio on Linux with S32G2 SDK - Problems</title>
      <link>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431469#M638</link>
      <description>&lt;P&gt;I have managed to install, it was just hidden in the CDT plugins page. Took an hour to install for some reason. Now I have the latest&amp;nbsp; examples.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Can_Do_bus_0-1647888942735.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174301iE2D2C988B5B00C64/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Can_Do_bus_0-1647888942735.png" alt="Can_Do_bus_0-1647888942735.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Mar 2022 18:56:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1431469#M638</guid>
      <dc:creator>Can_Do_bus</dc:creator>
      <dc:date>2022-03-21T18:56:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32 Design Studio on Linux with S32G2 SDK - Problems</title>
      <link>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1547945#M1635</link>
      <description>&lt;P&gt;The problem of not being able to download the RTD SDK, I found the solution.&lt;/P&gt;&lt;P&gt;Instead of using the default S32DS Extensions and Updates... , use the authentic "install new software" function of eclipse&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MarkZhou19_0-1667429485310.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/198970iA9F9C1FD56CBDB1E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MarkZhou19_0-1667429485310.png" alt="MarkZhou19_0-1667429485310.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MarkZhou19_1-1667429698754.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/198972i8A76EF55D88347AD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MarkZhou19_1-1667429698754.png" alt="MarkZhou19_1-1667429698754.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; Input this address, you'll find the sdk to download&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/lgfiles/updates/Eclipse/APSW/S32DS_3.4" target="_blank"&gt;http://www.nxp.com/lgfiles/updates/Eclipse/APSW/S32DS_3.4&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 22:55:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-Design-Studio-on-Linux-with-S32G2-SDK-Problems/m-p/1547945#M1635</guid>
      <dc:creator>MarkZhou19</dc:creator>
      <dc:date>2022-11-02T22:55:39Z</dc:date>
    </item>
  </channel>
</rss>