<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: LLCE, PFE memory allocation</title>
    <link>https://community.nxp.com/t5/S32G/LLCE-PFE-memory-allocation/m-p/1823434#M6188</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;All information available on regards of both NXP FW's is provided under their respective FW User Guide. On regards of an specific memory map for both FW's, we see that there is no available information, we do apologize. As for the following questions:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Also, is there space in LLCE and PFE that users can freely read and write?&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;We understand that LLCE-FW can also be provided as a Premium Software (not free), which provides customization (up to a certain point) for the developer. On regards of PFE-FW, we understand that there is not such kind of customization available, but there are additional features that can be enabled, but those features are provided directly by NXP.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Thu, 07 Mar 2024 14:26:37 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2024-03-07T14:26:37Z</dc:date>
    <item>
      <title>LLCE, PFE memory allocation</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-PFE-memory-allocation/m-p/1823304#M6184</link>
      <description>&lt;P&gt;I would like to know about the memory allocation of LLCE and PFE.&lt;/P&gt;&lt;P&gt;I would like to know about LLCE and PFE memory maps. Which document should I look at?&lt;/P&gt;&lt;P&gt;What you want to know is&lt;BR /&gt;LLCE shared memory address, LLCE CAN FIFO, shared memory location, RAM arrangement&lt;BR /&gt;I would like to know the PFE shared memory address and RAM layout.&lt;/P&gt;&lt;P&gt;Also, is there space in LLCE and PFE that users can freely read and write?&lt;/P&gt;</description>
      <pubDate>Thu, 07 Mar 2024 11:32:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-PFE-memory-allocation/m-p/1823304#M6184</guid>
      <dc:creator>kazuki</dc:creator>
      <dc:date>2024-03-07T11:32:25Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE, PFE memory allocation</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-PFE-memory-allocation/m-p/1823434#M6188</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;All information available on regards of both NXP FW's is provided under their respective FW User Guide. On regards of an specific memory map for both FW's, we see that there is no available information, we do apologize. As for the following questions:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Also, is there space in LLCE and PFE that users can freely read and write?&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;We understand that LLCE-FW can also be provided as a Premium Software (not free), which provides customization (up to a certain point) for the developer. On regards of PFE-FW, we understand that there is not such kind of customization available, but there are additional features that can be enabled, but those features are provided directly by NXP.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Mar 2024 14:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-PFE-memory-allocation/m-p/1823434#M6188</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-03-07T14:26:37Z</dc:date>
    </item>
  </channel>
</rss>