<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32ds NXP  build in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32ds-NXP-build/m-p/1816941#M6066</link>
    <description>&lt;P&gt;Hi Daniel Aguirre,&lt;/P&gt;&lt;P&gt;I use the S32DS_ARM_v2.2 platform, using this tool to compile my project is normal without error, but I use the command line to call NXP/S32DS_ARM_v2.2/eclipse.exe compilation will report the above error&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Wed, 28 Feb 2024 01:51:11 GMT</pubDate>
    <dc:creator>nancb</dc:creator>
    <dc:date>2024-02-28T01:51:11Z</dc:date>
    <item>
      <title>S32ds NXP  build</title>
      <link>https://community.nxp.com/t5/S32G/S32ds-NXP-build/m-p/1816302#M6054</link>
      <description>&lt;P&gt;I'm running a build from the command line and it generates the following errors&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.debug.&lt;/P&gt;&lt;P&gt;Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.release.&lt;/P&gt;&lt;P&gt;Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.debug.ram.&lt;/P&gt;&lt;P&gt;Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.executable.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.release.ram.&lt;/P&gt;&lt;P&gt;Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.static_library.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.debug.lib.&lt;/P&gt;&lt;P&gt;Managed Build system manifest file error: Unable to resolve the superClass identifier ghs.managedmake.arm.static_library.toolchain in the toolChain com.nxp.s32ds.cle.arm.mbs.ghs.toolchain.release.lib.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However everything builds correctly.&amp;nbsp; When I run this in an Azure DevOps pipeline it picks these up as errors, which I would prefer it didn't.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not sure where to even start looking for these, other than these look similar to the original build configuration names which we changed.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 08:00:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32ds-NXP-build/m-p/1816302#M6054</guid>
      <dc:creator>nancb</dc:creator>
      <dc:date>2024-02-27T08:00:42Z</dc:date>
    </item>
    <item>
      <title>Re: S32ds NXP  build</title>
      <link>https://community.nxp.com/t5/S32G/S32ds-NXP-build/m-p/1816598#M6059</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Can you let us know which S32 platform are you using? Also, which S32DS version are you working with?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 13:53:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32ds-NXP-build/m-p/1816598#M6059</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-02-27T13:53:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32ds NXP  build</title>
      <link>https://community.nxp.com/t5/S32G/S32ds-NXP-build/m-p/1816941#M6066</link>
      <description>&lt;P&gt;Hi Daniel Aguirre,&lt;/P&gt;&lt;P&gt;I use the S32DS_ARM_v2.2 platform, using this tool to compile my project is normal without error, but I use the command line to call NXP/S32DS_ARM_v2.2/eclipse.exe compilation will report the above error&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 01:51:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32ds-NXP-build/m-p/1816941#M6066</guid>
      <dc:creator>nancb</dc:creator>
      <dc:date>2024-02-28T01:51:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32ds NXP  build</title>
      <link>https://community.nxp.com/t5/S32G/S32ds-NXP-build/m-p/1817552#M6080</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback.&lt;/P&gt;
&lt;P&gt;Given the S32DS version you are using, it seems that this community might not be the correct one, since we mainly support S32G and related S32DS versions. We do apologize.&lt;/P&gt;
&lt;P&gt;Help us open this same request under the following community:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/bd-p/s32ds" target="_blank"&gt;S32 Design Studio - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Since in there you should receive the correct support. We also recommend detailing which S32 product you are using as well as if you are using any example or if it is only happening under non-NXP code.&lt;/P&gt;
&lt;P&gt;Again, we apologize.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 14:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32ds-NXP-build/m-p/1817552#M6080</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-02-28T14:07:20Z</dc:date>
    </item>
  </channel>
</rss>