<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: Wake On LAN for S32G3 / S32G-VNP-RDB3</title>
    <link>https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G3-S32G-VNP-RDB3/m-p/1816440#M6055</link>
    <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229914" target="_blank"&gt;jliu&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks for the reply and really sorry for late response&lt;/P&gt;
&lt;P&gt;Well, I have investigated the documents related and also confirmed with the internal team, this feature is not supported via GMAC/PFE.&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
    <pubDate>Tue, 27 Feb 2024 09:33:49 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2024-02-27T09:33:49Z</dc:date>
    <item>
      <title>Wake On LAN for S32G3 / S32G-VNP-RDB3</title>
      <link>https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G3-S32G-VNP-RDB3/m-p/1814082#M6001</link>
      <description>&lt;P class=""&gt;&lt;SPAN class=""&gt;We are using the GMAC interface for our RDB3 board and attempting to do wake on LAN.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;The KSZ9031 PHY connected to this interface supports wake on LAN upon configuration, however the GPIO interrupt from it does not connect to a wakeable pin on the RDB3 board so it cannot be used for wake on LAN.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Does the MAC itself support wake on LAN? Is there any documentation on how we can we configure it on the provided Linux BSP for the RDB3? It seems like when the RDB3 is put to sleep the PHY rail is powered off as well.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Feb 2024 20:01:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G3-S32G-VNP-RDB3/m-p/1814082#M6001</guid>
      <dc:creator>jlai</dc:creator>
      <dc:date>2024-02-22T20:01:22Z</dc:date>
    </item>
    <item>
      <title>Re: Wake On LAN for S32G3 / S32G-VNP-RDB3</title>
      <link>https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G3-S32G-VNP-RDB3/m-p/1814613#M6015</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229914" target="_blank"&gt;jliu&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks for the question.&lt;/P&gt;
&lt;P&gt;May I know which BSP version you are using now?&lt;/P&gt;
&lt;P&gt;Seems that this topic might have been discussed in the following link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G2-RDB2-Autolinux-BSP-v33/td-p/1608748" target="_blank"&gt;https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G2-RDB2-Autolinux-BSP-v33/td-p/1608748&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it could be helpful.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Fri, 23 Feb 2024 11:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G3-S32G-VNP-RDB3/m-p/1814613#M6015</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-02-23T11:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: Wake On LAN for S32G3 / S32G-VNP-RDB3</title>
      <link>https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G3-S32G-VNP-RDB3/m-p/1814924#M6021</link>
      <description>&lt;P&gt;We are using BSP version 38 with the RDB3.&lt;/P&gt;&lt;P&gt;Unfortunately the topic you linked does not provide additional information, it is not clear how to achieve Wake On LAN on the S32G3 RDB3 board. From the hardware schematics and documentation it seems like this is not possible on the S32G3 RDB3 board, could you please help confirm if it is and how to implement it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 24 Feb 2024 01:31:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G3-S32G-VNP-RDB3/m-p/1814924#M6021</guid>
      <dc:creator>jlai</dc:creator>
      <dc:date>2024-02-24T01:31:37Z</dc:date>
    </item>
    <item>
      <title>Re: Wake On LAN for S32G3 / S32G-VNP-RDB3</title>
      <link>https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G3-S32G-VNP-RDB3/m-p/1816440#M6055</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229914" target="_blank"&gt;jliu&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks for the reply and really sorry for late response&lt;/P&gt;
&lt;P&gt;Well, I have investigated the documents related and also confirmed with the internal team, this feature is not supported via GMAC/PFE.&lt;/P&gt;
&lt;P&gt;Sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 09:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Wake-On-LAN-for-S32G3-S32G-VNP-RDB3/m-p/1816440#M6055</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-02-27T09:33:49Z</dc:date>
    </item>
  </channel>
</rss>