<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32DS v3.5 Linux version not found RTD</title>
    <link>https://community.nxp.com/t5/S32G/S32DS-v3-5-Linux-version-not-found-RTD/m-p/1815494#M6032</link>
    <description>&lt;P&gt;Hi expert,&lt;/P&gt;&lt;P&gt;I'm using S32DS to do DDR training test.&lt;BR /&gt;I install S32DS v3.5 linux version on Ubuntu20.04 system following&amp;nbsp;&lt;SPAN&gt;Installation Guide, and it startup&amp;amp;run Okay.&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;But I find that there is no RTD package in the "Extentions and Upates" window.&lt;BR /&gt;Then I install the same version(v3.5) on Windows 10 system, and I&amp;nbsp;find that there is RTD v4.0.0 package in the "Extentions and Upate" window, and it can be installed.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;I compare the "Avalilable S32DS Software Sites" of Preferences menu, but there is no difference.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does Linux version of S32DS no RTD package? Or I miss something?&lt;BR /&gt;I want to install RTD to the S32DS in Ubuntu system to do DDR training test. But I don't know how and where to install it.&lt;BR /&gt;Could you help me please ?&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 26 Feb 2024 10:26:17 GMT</pubDate>
    <dc:creator>jack_zhangjg</dc:creator>
    <dc:date>2024-02-26T10:26:17Z</dc:date>
    <item>
      <title>S32DS v3.5 Linux version not found RTD</title>
      <link>https://community.nxp.com/t5/S32G/S32DS-v3-5-Linux-version-not-found-RTD/m-p/1815494#M6032</link>
      <description>&lt;P&gt;Hi expert,&lt;/P&gt;&lt;P&gt;I'm using S32DS to do DDR training test.&lt;BR /&gt;I install S32DS v3.5 linux version on Ubuntu20.04 system following&amp;nbsp;&lt;SPAN&gt;Installation Guide, and it startup&amp;amp;run Okay.&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;But I find that there is no RTD package in the "Extentions and Upates" window.&lt;BR /&gt;Then I install the same version(v3.5) on Windows 10 system, and I&amp;nbsp;find that there is RTD v4.0.0 package in the "Extentions and Upate" window, and it can be installed.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;I compare the "Avalilable S32DS Software Sites" of Preferences menu, but there is no difference.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does Linux version of S32DS no RTD package? Or I miss something?&lt;BR /&gt;I want to install RTD to the S32DS in Ubuntu system to do DDR training test. But I don't know how and where to install it.&lt;BR /&gt;Could you help me please ?&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 10:26:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32DS-v3-5-Linux-version-not-found-RTD/m-p/1815494#M6032</guid>
      <dc:creator>jack_zhangjg</dc:creator>
      <dc:date>2024-02-26T10:26:17Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS v3.5 Linux version not found RTD</title>
      <link>https://community.nxp.com/t5/S32G/S32DS-v3-5-Linux-version-not-found-RTD/m-p/1815664#M6039</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the following information:&lt;/P&gt;
&lt;P&gt;"&lt;SPAN&gt;I compare the "Avalilable S32DS Software Sites" of Preferences menu, but there is no difference.&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;We understand that there might be a problem where S32DS is not being able to connect to the available sites under Linux. Can you let us know which S32 variant you are working with?&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 14:32:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32DS-v3-5-Linux-version-not-found-RTD/m-p/1815664#M6039</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-02-26T14:32:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS v3.5 Linux version not found RTD</title>
      <link>https://community.nxp.com/t5/S32G/S32DS-v3-5-Linux-version-not-found-RTD/m-p/2002177#M11861</link>
      <description>&lt;P&gt;I am having the exact problem.&lt;/P&gt;&lt;P&gt;I've installed S32DS 3.5 update 13 in Windows and Linux.&amp;nbsp; I've installed the development package for the&amp;nbsp;S32K3xx processor, then attempted the installation for the RTD drivers.&amp;nbsp; In Windows, everything works fine.&amp;nbsp; In Linux, although the installation completes, I do not see the RTD drivers listed in the "Extensions and Updates" window.&amp;nbsp; Nor do I see any examples with the RD version I am attempting to load.&lt;/P&gt;&lt;P&gt;What was the resolution to this issue?&amp;nbsp; Is there an issue using the RTD drivers in S32DS under Linux?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using Ubuntu 20.04,&amp;nbsp;SW32K3_S32DS_3.5.13_D2407.zip, and&amp;nbsp;SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.zip.&lt;/P&gt;&lt;P&gt;I need Linux support because my Windows environment in VirtualBox does not work with the Multilink debugger.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Nov 2024 18:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32DS-v3-5-Linux-version-not-found-RTD/m-p/2002177#M11861</guid>
      <dc:creator>adalberto1</dc:creator>
      <dc:date>2024-11-26T18:13:01Z</dc:date>
    </item>
  </channel>
</rss>