<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Lauterbach script in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Lauterbach-script/m-p/1812382#M5979</link>
    <description>&lt;P&gt;Hello , i tried to attach a lauterbach script for s32g3 rdb3. I have been getting an error saying "Target processor in reset". Can you please let me know what the error is and also which script to install.&lt;BR /&gt;&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Wed, 21 Feb 2024 03:33:07 GMT</pubDate>
    <dc:creator>Abhiram_m_s</dc:creator>
    <dc:date>2024-02-21T03:33:07Z</dc:date>
    <item>
      <title>Lauterbach script</title>
      <link>https://community.nxp.com/t5/S32G/Lauterbach-script/m-p/1812382#M5979</link>
      <description>&lt;P&gt;Hello , i tried to attach a lauterbach script for s32g3 rdb3. I have been getting an error saying "Target processor in reset". Can you please let me know what the error is and also which script to install.&lt;BR /&gt;&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 03:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Lauterbach-script/m-p/1812382#M5979</guid>
      <dc:creator>Abhiram_m_s</dc:creator>
      <dc:date>2024-02-21T03:33:07Z</dc:date>
    </item>
    <item>
      <title>Re: Lauterbach script</title>
      <link>https://community.nxp.com/t5/S32G/Lauterbach-script/m-p/1813304#M5988</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229803" target="_blank"&gt;Abhiram_m_s&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks for the question.&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Regarding to the "Target processor in reset", the following link would be the official reference: &lt;A href="https://support.lauterbach.com/kb/articles/arm-system-up-system-mode-attach-returns-target-reset-detected" target="_blank"&gt;https://support.lauterbach.com/kb/articles/arm-system-up-system-mode-attach-returns-target-reset-detected&lt;/A&gt;&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;You may try to disconnect the debug cable and reconnect with the board powered off, then power on the board and check if the problem persists.&lt;/P&gt;
&lt;OL start="2"&gt;
&lt;LI&gt;Regarding to the script, it depends on which package/examples you are using, in general, &amp;nbsp;in the RTD SW package, there would be cmm file existed for debugging.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;For example, if you are working with the Integration Reference Examples, the following scripts could be used for reference: Integration_Reference_Examples_S32G3_2023_02\code\framework\realtime\swc\bootloader\platforms\S32G3XX\build\cmm&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Thu, 22 Feb 2024 02:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Lauterbach-script/m-p/1813304#M5988</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-02-22T02:33:26Z</dc:date>
    </item>
  </channel>
</rss>