<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic about QSPI NOR flash lock/unlock in S32G</title>
    <link>https://community.nxp.com/t5/S32G/about-QSPI-NOR-flash-lock-unlock/m-p/1811681#M5971</link>
    <description>&lt;P&gt;I'm trying to lock QSPI Flash.&lt;/P&gt;&lt;P&gt;Test on s32g274ardb2 board with bsp39. But when run command "flash_lock -i /dev/mtd0", it return error like this:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;flash_lock: error!: could not check lock status device: /dev/mtd0&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;error 95 (Operation not supported)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;It seems flash_lock operation doesn't supported by this driver.&lt;/P&gt;&lt;P&gt;However, flash_erase is OK.&lt;/P&gt;&lt;P&gt;I also try sf protect lock in u-boot. It doesn't work too.&lt;/P&gt;&lt;P&gt;So is NOR flash lock operation supported on current S32G BSP?&lt;/P&gt;&lt;P&gt;Thansk!&lt;/P&gt;</description>
    <pubDate>Tue, 20 Feb 2024 08:57:08 GMT</pubDate>
    <dc:creator>Guangyu_D</dc:creator>
    <dc:date>2024-02-20T08:57:08Z</dc:date>
    <item>
      <title>about QSPI NOR flash lock/unlock</title>
      <link>https://community.nxp.com/t5/S32G/about-QSPI-NOR-flash-lock-unlock/m-p/1811681#M5971</link>
      <description>&lt;P&gt;I'm trying to lock QSPI Flash.&lt;/P&gt;&lt;P&gt;Test on s32g274ardb2 board with bsp39. But when run command "flash_lock -i /dev/mtd0", it return error like this:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;flash_lock: error!: could not check lock status device: /dev/mtd0&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;error 95 (Operation not supported)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;It seems flash_lock operation doesn't supported by this driver.&lt;/P&gt;&lt;P&gt;However, flash_erase is OK.&lt;/P&gt;&lt;P&gt;I also try sf protect lock in u-boot. It doesn't work too.&lt;/P&gt;&lt;P&gt;So is NOR flash lock operation supported on current S32G BSP?&lt;/P&gt;&lt;P&gt;Thansk!&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 08:57:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/about-QSPI-NOR-flash-lock-unlock/m-p/1811681#M5971</guid>
      <dc:creator>Guangyu_D</dc:creator>
      <dc:date>2024-02-20T08:57:08Z</dc:date>
    </item>
    <item>
      <title>Re: about QSPI NOR flash lock/unlock</title>
      <link>https://community.nxp.com/t5/S32G/about-QSPI-NOR-flash-lock-unlock/m-p/1812507#M5981</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226420" target="_blank" rel="noopener"&gt;Guangyu_D&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks for the question.&lt;/P&gt;
&lt;P&gt;I have checked the BSP user manual, as well as the latest code in kernel drivers, the locking operations are not supported, hence the flash_lock utility cannot be used.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 06:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/about-QSPI-NOR-flash-lock-unlock/m-p/1812507#M5981</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-02-21T06:35:36Z</dc:date>
    </item>
  </channel>
</rss>