<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G274 U-Boot boot linux kernel Failed in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1810985#M5958</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback. For the behavior you are mentioning, it seems that you are re-initializing the pin configuration, hence it is creating problems with your application.&lt;/P&gt;
&lt;P&gt;When working with multicore applications, the shared resources should only be initialized once (i.e. clocks, pins), if not then non-defined behavior may happen (as you are seeing).&lt;/P&gt;
&lt;P&gt;The following document provides a reference on regard of the shared resources management under S32G2:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-Bootloader-Customzition/ta-p/1519838" target="_blank" rel="noopener"&gt;S32G Bootloader Customzition - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Again, this only provides a reference. We understand that it does not cover all shared resources available under the S32G.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Mon, 19 Feb 2024 14:33:05 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2024-02-19T14:33:05Z</dc:date>
    <item>
      <title>S32G274 U-Boot boot linux kernel Failed</title>
      <link>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1803046#M5876</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;expert:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;U-boot boot linux kernel failed by command "boot",&amp;nbsp; error info as below picture;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Archieeeee_0-1707267850672.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/262243iABEAE7333FF4014B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Archieeeee_0-1707267850672.jpeg" alt="Archieeeee_0-1707267850672.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;as picture, S32G274 boot by SD card; and u-boot boot m7 core0 by command "startm7"&lt;/P&gt;&lt;P&gt;M7&amp;nbsp;is running normally，after "startm7", enter command "boot",&amp;nbsp; the kernel report error;&lt;/P&gt;&lt;P&gt;But, when i not startm7, u-boot can boot linux kernel normal;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so i think it's some&amp;nbsp;conflict，&lt;/P&gt;&lt;P&gt;M7 code is below pictrue,&amp;nbsp;I am already disabled the Clock init and port init&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 931px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/262246iB78FD0CCCBA16938/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;M7 address range is 0x34000000-0x3453FFFF&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 665px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/262247i6F619F52B7547494/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pls help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Feb 2024 01:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1803046#M5876</guid>
      <dc:creator>Archieeeee</dc:creator>
      <dc:date>2024-02-07T01:17:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32G274 U-Boot boot linux kernel Failed</title>
      <link>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1803555#M5884</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Which BSP version are you using? Was it modified?&lt;/P&gt;
&lt;P&gt;The bootflow that you are using is not recommended by NXP (there is no documentation for it). Still, there is an example that uses this same bootflow (IPCF example). We can recommend verifying that you are able to load the IPCF example and run it properly then start looking into modifications.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Feb 2024 17:28:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1803555#M5884</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-02-07T17:28:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32G274 U-Boot boot linux kernel Failed</title>
      <link>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1804116#M5893</link>
      <description>&lt;P&gt;Hi, Daniel:&lt;/P&gt;&lt;P&gt;Thanks for you reply,&amp;nbsp;&lt;/P&gt;&lt;P&gt;The BSP Version is "BSP 39.0" ,i git clone from&amp;nbsp;&lt;A href="https://github.com/nxp-auto-linux/auto_yocto_bsp/tree/release/bsp39.0" target="_blank"&gt;https://github.com/nxp-auto-linux/auto_yocto_bsp/tree/release/bsp39.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;could you tell me the path of IPCF example, i found&amp;nbsp;Ipcf_Example_S32G274A_M7 &amp;nbsp;that path :D:\NXP\SW32G_IPCF_4.8.0_D2212\eclipse\plugins\Ipcf_TS_T40D11M40I0R0\examples\EBT\S32G2\Ipcf_Example_S32G274A_M7&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;could you upload a ipcf example, and what modifications are needed for BSP, which doc&amp;nbsp;describe the modification&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Feb 2024 13:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1804116#M5893</guid>
      <dc:creator>Archieeeee</dc:creator>
      <dc:date>2024-02-08T13:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32G274 U-Boot boot linux kernel Failed</title>
      <link>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1804315#M5903</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;That is one option, which is using EB Tresos. More detailed description is provided under the "description.txt" file available under the example.&lt;/P&gt;
&lt;P&gt;We can recommend using the S32DS example, since we see it as a more straightforward option due to no additional configuration required (just having the pre-requisites for the package).&lt;/P&gt;
&lt;P&gt;Still, both options should work.&lt;/P&gt;
&lt;P&gt;As for uploading examples, we don't commonly provide examples through the community, we do apologize.&lt;/P&gt;
&lt;P&gt;On regards of changes to the BSP, no changes are required, aside from the commands shown under the "description.txt" file.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Feb 2024 17:57:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1804315#M5903</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-02-08T17:57:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32G274 U-Boot boot linux kernel Failed</title>
      <link>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1810370#M5948</link>
      <description>&lt;P&gt;Hi，Daniel:&lt;/P&gt;&lt;P&gt;I'm sorry for the late reply，I'm fix the issue by remake the sd card; now M7_Core 0 can boot&amp;nbsp; normal;&lt;/P&gt;&lt;P&gt;and the linux kernel boot normal;&lt;/P&gt;&lt;P&gt;but when i enable port_init in m7 core project. as line 59 code in the blow picture&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Archieeeee_0-1708244573803.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263588i7CC9910C56575B85/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Archieeeee_0-1708244573803.png" alt="Archieeeee_0-1708244573803.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;the u-boot uart will be&amp;nbsp; failure,&amp;nbsp; u-boot use uart0;&lt;/P&gt;&lt;P&gt;and i'm configed the uart0 port in mcal;&lt;/P&gt;&lt;P&gt;maybe some config confict in mcal or u-boot&lt;/P&gt;&lt;P&gt;how do i solved the gpio config confict in mcal and u-boot/linux&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pls Help&lt;/P&gt;</description>
      <pubDate>Sun, 18 Feb 2024 08:27:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1810370#M5948</guid>
      <dc:creator>Archieeeee</dc:creator>
      <dc:date>2024-02-18T08:27:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32G274 U-Boot boot linux kernel Failed</title>
      <link>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1810985#M5958</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thanks for your feedback. For the behavior you are mentioning, it seems that you are re-initializing the pin configuration, hence it is creating problems with your application.&lt;/P&gt;
&lt;P&gt;When working with multicore applications, the shared resources should only be initialized once (i.e. clocks, pins), if not then non-defined behavior may happen (as you are seeing).&lt;/P&gt;
&lt;P&gt;The following document provides a reference on regard of the shared resources management under S32G2:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/S32G-Bootloader-Customzition/ta-p/1519838" target="_blank" rel="noopener"&gt;S32G Bootloader Customzition - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Again, this only provides a reference. We understand that it does not cover all shared resources available under the S32G.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Feb 2024 14:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G274-U-Boot-boot-linux-kernel-Failed/m-p/1810985#M5958</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-02-19T14:33:05Z</dc:date>
    </item>
  </channel>
</rss>