<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックGetting to work Safety Peripheral Drivers example</title>
    <link>https://community.nxp.com/t5/S32G/Getting-to-work-Safety-Peripheral-Drivers-example/m-p/1425870#M595</link>
    <description>&lt;P&gt;I have installed SPD 1.01 as part of the Automative Software Package Manager bundle. But I could not get SPD example to work, configuration tools throws an error as:&lt;/P&gt;&lt;P&gt;Issue: Processor '' detected in NXP GCC 9.2 for Arm 32-bit Bare-Metal project does not match with currently selected `S32G274A_Rev2`. Target processor not supported or the computer is not on-line.&lt;BR /&gt;Level: Error&lt;BR /&gt;Type: Tool problem&lt;BR /&gt;Tool: McuConfiguration&lt;BR /&gt;Origin: SPD_101_S32G274_Rev2_M7_0&lt;BR /&gt;Resource: Processor&lt;BR /&gt;Information: -&lt;/P&gt;&lt;P&gt;Furthermore, the main.c in the example is empty (only the template main is there). Is there anyone having the same issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Mar 2022 06:25:58 GMT</pubDate>
    <dc:creator>halilmutlu</dc:creator>
    <dc:date>2022-03-10T06:25:58Z</dc:date>
    <item>
      <title>Getting to work Safety Peripheral Drivers example</title>
      <link>https://community.nxp.com/t5/S32G/Getting-to-work-Safety-Peripheral-Drivers-example/m-p/1425870#M595</link>
      <description>&lt;P&gt;I have installed SPD 1.01 as part of the Automative Software Package Manager bundle. But I could not get SPD example to work, configuration tools throws an error as:&lt;/P&gt;&lt;P&gt;Issue: Processor '' detected in NXP GCC 9.2 for Arm 32-bit Bare-Metal project does not match with currently selected `S32G274A_Rev2`. Target processor not supported or the computer is not on-line.&lt;BR /&gt;Level: Error&lt;BR /&gt;Type: Tool problem&lt;BR /&gt;Tool: McuConfiguration&lt;BR /&gt;Origin: SPD_101_S32G274_Rev2_M7_0&lt;BR /&gt;Resource: Processor&lt;BR /&gt;Information: -&lt;/P&gt;&lt;P&gt;Furthermore, the main.c in the example is empty (only the template main is there). Is there anyone having the same issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 06:25:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Getting-to-work-Safety-Peripheral-Drivers-example/m-p/1425870#M595</guid>
      <dc:creator>halilmutlu</dc:creator>
      <dc:date>2022-03-10T06:25:58Z</dc:date>
    </item>
  </channel>
</rss>