<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32G bootloader example project code is missing for S32DS</title>
    <link>https://community.nxp.com/t5/S32G/S32G-bootloader-example-project-code-is-missing-for-S32DS/m-p/1809832#M5935</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i am trying to customize a project specific bootloader from the S32G bootloader example that provided in "Integration_Reference_Examples". as i read the "UM_BOOTLOADER_Rev_2023.05", in chapter 3, "release layout" it seems imply that there is an already defined S32DS project for the bootloader, however, i can only find the Tesos workspace for the bootloader.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;lt;package_installation_folder&amp;gt;/applications/realtime/S32DS/&lt;BR /&gt;workspaces/&amp;lt;workspace_name&amp;gt; - contains the S32 Design Studio workspace for a certain example (e.g.&lt;BR /&gt;Bootloader, Lighting etc.).&lt;/P&gt;&lt;P&gt;can anyone tell me how can i find the S32DS project/workspace for the bootloader example? or must i use Tesos to create the project?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 16 Feb 2024 08:28:40 GMT</pubDate>
    <dc:creator>marvin_wang</dc:creator>
    <dc:date>2024-02-16T08:28:40Z</dc:date>
    <item>
      <title>S32G bootloader example project code is missing for S32DS</title>
      <link>https://community.nxp.com/t5/S32G/S32G-bootloader-example-project-code-is-missing-for-S32DS/m-p/1809832#M5935</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i am trying to customize a project specific bootloader from the S32G bootloader example that provided in "Integration_Reference_Examples". as i read the "UM_BOOTLOADER_Rev_2023.05", in chapter 3, "release layout" it seems imply that there is an already defined S32DS project for the bootloader, however, i can only find the Tesos workspace for the bootloader.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;lt;package_installation_folder&amp;gt;/applications/realtime/S32DS/&lt;BR /&gt;workspaces/&amp;lt;workspace_name&amp;gt; - contains the S32 Design Studio workspace for a certain example (e.g.&lt;BR /&gt;Bootloader, Lighting etc.).&lt;/P&gt;&lt;P&gt;can anyone tell me how can i find the S32DS project/workspace for the bootloader example? or must i use Tesos to create the project?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Feb 2024 08:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-bootloader-example-project-code-is-missing-for-S32DS/m-p/1809832#M5935</guid>
      <dc:creator>marvin_wang</dc:creator>
      <dc:date>2024-02-16T08:28:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32G bootloader example project code is missing for S32DS</title>
      <link>https://community.nxp.com/t5/S32G/S32G-bootloader-example-project-code-is-missing-for-S32DS/m-p/1810112#M5941</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We understand that you downloaded the *.exe file and installed it in your computer, is this correct?&lt;/P&gt;
&lt;P&gt;If so, there is an *.updatesite file (aside from the *.exe) which is available under the same page:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DanielAguirre_0-1708099199539.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263525i7AAA226E79F5A560/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DanielAguirre_0-1708099199539.png" alt="DanielAguirre_0-1708099199539.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If all requirements are fulfilled under S32DS, you should be able to add the *.updatesite file and install the plugin for the project to be available under S32DS.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Feb 2024 16:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-bootloader-example-project-code-is-missing-for-S32DS/m-p/1810112#M5941</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2024-02-16T16:00:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32G bootloader example project code is missing for S32DS</title>
      <link>https://community.nxp.com/t5/S32G/S32G-bootloader-example-project-code-is-missing-for-S32DS/m-p/1810324#M5944</link>
      <description>Thanks, i have downloaded that and it works</description>
      <pubDate>Sat, 17 Feb 2024 13:16:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-bootloader-example-project-code-is-missing-for-S32DS/m-p/1810324#M5944</guid>
      <dc:creator>marvin_wang</dc:creator>
      <dc:date>2024-02-17T13:16:43Z</dc:date>
    </item>
  </channel>
</rss>