<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32G Yocto Build Issue: critical programs are missing or too old: GNU ld in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G-Yocto-Build-Issue-critical-programs-are-missing-or-too-old/m-p/1425428#M588</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on Ubuntu 18.04. I am following the document&amp;nbsp;S32G274A_LinuxBSP28.0.0_User_Manual.pdf for building Yocto BSP For S32G274A.&lt;/P&gt;&lt;P&gt;I have installed all the packages required for YOcto build.I am getting following error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;| checking version of gawk... 4.1.4, ok&lt;BR /&gt;| checking for bison... bison&lt;BR /&gt;| checking version of bison... 3.7.2, ok&lt;BR /&gt;| checking if aarch64-fsl-linux-gcc --sysroot=/home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/recipe-sysroot is sufficient to build libc... yes&lt;BR /&gt;| checking for aarch64-fsl-linux-nm... aarch64-fsl-linux-nm&lt;BR /&gt;| checking for python3... python3&lt;BR /&gt;| checking version of python3... 3.6.9, ok&lt;BR /&gt;| configure: error:&lt;BR /&gt;&lt;STRONG&gt;| *** These critical programs are missing or too old: GNU ld&lt;/STRONG&gt;&lt;BR /&gt;| *** Check the INSTALL file for required versions.&lt;BR /&gt;| WARNING: /home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_configure.24760:211 exit 1 from 'exit 1'&lt;BR /&gt;| WARNING: Backtrace (BB generated script):&lt;BR /&gt;| #1: bbfatal_log, /home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_configure.24760, line 211&lt;BR /&gt;| #2: oe_runconf, /home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_configure.24760, line 173&lt;BR /&gt;| #3: do_configure, /home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_configure.24760, line 160&lt;BR /&gt;| #4: main, /home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_configure.24760, line 215&lt;BR /&gt;|&lt;BR /&gt;| Backtrace (metadata-relative locations):&lt;BR /&gt;| #1: bbfatal_log, /home/deepika/fsl-auto-yocto-bsp/sources/poky/meta/classes/logging.bbclass, line 72&lt;BR /&gt;| #2: oe_runconf, /home/deepika/fsl-auto-yocto-bsp/sources/poky/meta/classes/autotools.bbclass, line 96&lt;BR /&gt;| #3: do_configure, /home/deepika/fsl-auto-yocto-bsp/sources/poky/meta/recipes-core/glibc/glibc_2.32.bb, line 101&lt;BR /&gt;ERROR: Task (/home/deepika/fsl-auto-yocto-bsp/sources/poky/meta/recipes-core/glibc/glibc_2.32.bb:do_configure) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 1680 tasks of which 1374 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;From the logs it looks like GNU ld version can be one problem.I installed binutils 2.28 in the host machine.But problem persists.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest any solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Deepika&lt;/P&gt;</description>
    <pubDate>Wed, 09 Mar 2022 16:36:36 GMT</pubDate>
    <dc:creator>deepika_t</dc:creator>
    <dc:date>2022-03-09T16:36:36Z</dc:date>
    <item>
      <title>S32G Yocto Build Issue: critical programs are missing or too old: GNU ld</title>
      <link>https://community.nxp.com/t5/S32G/S32G-Yocto-Build-Issue-critical-programs-are-missing-or-too-old/m-p/1425428#M588</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on Ubuntu 18.04. I am following the document&amp;nbsp;S32G274A_LinuxBSP28.0.0_User_Manual.pdf for building Yocto BSP For S32G274A.&lt;/P&gt;&lt;P&gt;I have installed all the packages required for YOcto build.I am getting following error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;| checking version of gawk... 4.1.4, ok&lt;BR /&gt;| checking for bison... bison&lt;BR /&gt;| checking version of bison... 3.7.2, ok&lt;BR /&gt;| checking if aarch64-fsl-linux-gcc --sysroot=/home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/recipe-sysroot is sufficient to build libc... yes&lt;BR /&gt;| checking for aarch64-fsl-linux-nm... aarch64-fsl-linux-nm&lt;BR /&gt;| checking for python3... python3&lt;BR /&gt;| checking version of python3... 3.6.9, ok&lt;BR /&gt;| configure: error:&lt;BR /&gt;&lt;STRONG&gt;| *** These critical programs are missing or too old: GNU ld&lt;/STRONG&gt;&lt;BR /&gt;| *** Check the INSTALL file for required versions.&lt;BR /&gt;| WARNING: /home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_configure.24760:211 exit 1 from 'exit 1'&lt;BR /&gt;| WARNING: Backtrace (BB generated script):&lt;BR /&gt;| #1: bbfatal_log, /home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_configure.24760, line 211&lt;BR /&gt;| #2: oe_runconf, /home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_configure.24760, line 173&lt;BR /&gt;| #3: do_configure, /home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_configure.24760, line 160&lt;BR /&gt;| #4: main, /home/deepika/fsl-auto-yocto-bsp/build_s32g274aevb/tmp/work/aarch64-fsl-linux/glibc/2.32-r0/temp/run.do_configure.24760, line 215&lt;BR /&gt;|&lt;BR /&gt;| Backtrace (metadata-relative locations):&lt;BR /&gt;| #1: bbfatal_log, /home/deepika/fsl-auto-yocto-bsp/sources/poky/meta/classes/logging.bbclass, line 72&lt;BR /&gt;| #2: oe_runconf, /home/deepika/fsl-auto-yocto-bsp/sources/poky/meta/classes/autotools.bbclass, line 96&lt;BR /&gt;| #3: do_configure, /home/deepika/fsl-auto-yocto-bsp/sources/poky/meta/recipes-core/glibc/glibc_2.32.bb, line 101&lt;BR /&gt;ERROR: Task (/home/deepika/fsl-auto-yocto-bsp/sources/poky/meta/recipes-core/glibc/glibc_2.32.bb:do_configure) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 1680 tasks of which 1374 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;From the logs it looks like GNU ld version can be one problem.I installed binutils 2.28 in the host machine.But problem persists.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest any solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Deepika&lt;/P&gt;</description>
      <pubDate>Wed, 09 Mar 2022 16:36:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-Yocto-Build-Issue-critical-programs-are-missing-or-too-old/m-p/1425428#M588</guid>
      <dc:creator>deepika_t</dc:creator>
      <dc:date>2022-03-09T16:36:36Z</dc:date>
    </item>
    <item>
      <title>Re: S32G Yocto Build Issue: critical programs are missing or too old: GNU ld</title>
      <link>https://community.nxp.com/t5/S32G/S32G-Yocto-Build-Issue-critical-programs-are-missing-or-too-old/m-p/1426215#M598</link>
      <description>&lt;P&gt;Hello deepika_t,&lt;/P&gt;
&lt;P&gt;You probably miss some installation packages of the host, because it is working perfectly on my design, the GCC is not the issue maybe some package itself.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.yoctoproject.org/docs/current/ref-manual/ref-manual.html" target="_blank"&gt;https://www.yoctoproject.org/docs/current/ref-manual/ref-manual.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 14:32:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-Yocto-Build-Issue-critical-programs-are-missing-or-too-old/m-p/1426215#M598</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-03-10T14:32:41Z</dc:date>
    </item>
  </channel>
</rss>