<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s32g image build in S32G</title>
    <link>https://community.nxp.com/t5/S32G/s32g-image-build/m-p/1803201#M5879</link>
    <description>&lt;P&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226643"&gt;@athul_am&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Thank you for the reply.&lt;/P&gt;
&lt;P&gt;As far as I know, the ubuntu version is 20.04 before BSP36 by default, if you would use the BSP36 or newer one, the default one is 22.04, If targeting Ubuntu-20.04 images on these newer BSPs, add the following line in /conf/local.conf.&lt;/P&gt;
&lt;P&gt;UBUNTU_TARGET_VERSION = "20.04.1"&lt;/P&gt;
&lt;P&gt;Currently for building BSPs, I suggest using the command listed in the BSP user manual for building the Ubuntu based images, in details described in chapter 3.1.3: BSP ubuntu build.&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
    <pubDate>Wed, 07 Feb 2024 07:39:18 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2024-02-07T07:39:18Z</dc:date>
    <item>
      <title>s32g image build</title>
      <link>https://community.nxp.com/t5/S32G/s32g-image-build/m-p/1801759#M5863</link>
      <description>&lt;P&gt;hi ,&lt;/P&gt;&lt;P&gt;Can someone let me know the steps to build an ubuntu image for Nxp s32grdb2.I need to enable all ethernet ports in the image also.&lt;/P&gt;&lt;P&gt;The manual i have is bsp 28.0 version and after the repo migration it is not working.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in Advance&lt;/P&gt;</description>
      <pubDate>Mon, 05 Feb 2024 08:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g-image-build/m-p/1801759#M5863</guid>
      <dc:creator>athul_am</dc:creator>
      <dc:date>2024-02-05T08:54:09Z</dc:date>
    </item>
    <item>
      <title>Re: s32g image build</title>
      <link>https://community.nxp.com/t5/S32G/s32g-image-build/m-p/1802266#M5869</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226643" target="_blank"&gt;athul_am&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks for the questions.&lt;/P&gt;
&lt;P&gt;BSP28 is relatively old, you may carefully reference the following link for the details:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32G-Knowledge-Base/How-to-build-older-Auto-Linux-BSPs/ta-p/1637516" target="_blank"&gt;https://community.nxp.com/t5/S32G-Knowledge-Base/How-to-build-older-Auto-Linux-BSPs/ta-p/1637516&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I tried the following command according to the BSP user manual and seems it could start the building without issues:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;git clone &lt;A href="https://github.com/nxp-auto-linux/linux-bsp-utils.git" target="_blank"&gt;https://github.com/nxp-auto-linux/linux-bsp-utils.git&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;cd linux-bsp-utils/codeaurora_migration/&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;./migrate.sh --full --work_path ./BSP28 --release_branch release/bsp28.0&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;cd BSP28/auto-bsp/&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;./sources/meta-alb/scripts/host-prepare.sh&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;. nxp-setup-alb.sh -m s32g274ardb2ubuntu&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;cd build_s32g274ardb2ubuntu&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;bitbake fsl-image-ubuntu-base&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You may help to try it on your own building machines&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 03:13:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g-image-build/m-p/1802266#M5869</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-02-06T03:13:34Z</dc:date>
    </item>
    <item>
      <title>Re: s32g image build</title>
      <link>https://community.nxp.com/t5/S32G/s32g-image-build/m-p/1803070#M5877</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24163"&gt;@chenyin_h&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thank you for the Response it is not mandatory that i use the 28 version i can use the latest version also,&lt;/P&gt;&lt;P&gt;my usecase is to build an image for the s32grdb2 board with all the ports enabled. I would like to build the fsl-image-bluebox as it was used in earlier boards but it gives me error that i need the ubuntu 20.04 and not 22.04. Is there any issue with that image regarding the ubuntu version.&lt;/P&gt;&lt;P&gt;Sorry if the above question is something dumb.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Athul&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Feb 2024 02:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g-image-build/m-p/1803070#M5877</guid>
      <dc:creator>athul_am</dc:creator>
      <dc:date>2024-02-07T02:26:40Z</dc:date>
    </item>
    <item>
      <title>Re: s32g image build</title>
      <link>https://community.nxp.com/t5/S32G/s32g-image-build/m-p/1803201#M5879</link>
      <description>&lt;P&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226643"&gt;@athul_am&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Thank you for the reply.&lt;/P&gt;
&lt;P&gt;As far as I know, the ubuntu version is 20.04 before BSP36 by default, if you would use the BSP36 or newer one, the default one is 22.04, If targeting Ubuntu-20.04 images on these newer BSPs, add the following line in /conf/local.conf.&lt;/P&gt;
&lt;P&gt;UBUNTU_TARGET_VERSION = "20.04.1"&lt;/P&gt;
&lt;P&gt;Currently for building BSPs, I suggest using the command listed in the BSP user manual for building the Ubuntu based images, in details described in chapter 3.1.3: BSP ubuntu build.&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 07 Feb 2024 07:39:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g-image-build/m-p/1803201#M5879</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-02-07T07:39:18Z</dc:date>
    </item>
  </channel>
</rss>