<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックERR050481 on S32G274A-RDB2</title>
    <link>https://community.nxp.com/t5/S32G/ERR050481-on-S32G274A-RDB2/m-p/1791626#M5719</link>
    <description>&lt;P&gt;Hello! I am trying to boot QNX 7.1.0 on board s32g274a-rdb2 and I am running into an issue that seems to be caused by ERR050481(boot works fine when booting only on one or 2 cores meaning the first cluster, but fails when the second cluster is involved). I have the Linux BSP 29 provided by NXP for this board and the U-Boot that comes with it. My question is, does U-boot do the necessary workaround for this erratum, or should the QNX startup code implement it?&lt;/P&gt;&lt;P&gt;My guess is that it does, since during Linux startup I do not seem to get a message regarding TLBI being handled incorrectly so I would hope that the handling is done by U-Boot, but I would appreciate a confirmation whether that is truly the case. Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Fri, 19 Jan 2024 06:15:23 GMT</pubDate>
    <dc:creator>TudorMorosanu</dc:creator>
    <dc:date>2024-01-19T06:15:23Z</dc:date>
    <item>
      <title>ERR050481 on S32G274A-RDB2</title>
      <link>https://community.nxp.com/t5/S32G/ERR050481-on-S32G274A-RDB2/m-p/1791626#M5719</link>
      <description>&lt;P&gt;Hello! I am trying to boot QNX 7.1.0 on board s32g274a-rdb2 and I am running into an issue that seems to be caused by ERR050481(boot works fine when booting only on one or 2 cores meaning the first cluster, but fails when the second cluster is involved). I have the Linux BSP 29 provided by NXP for this board and the U-Boot that comes with it. My question is, does U-boot do the necessary workaround for this erratum, or should the QNX startup code implement it?&lt;/P&gt;&lt;P&gt;My guess is that it does, since during Linux startup I do not seem to get a message regarding TLBI being handled incorrectly so I would hope that the handling is done by U-Boot, but I would appreciate a confirmation whether that is truly the case. Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jan 2024 06:15:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/ERR050481-on-S32G274A-RDB2/m-p/1791626#M5719</guid>
      <dc:creator>TudorMorosanu</dc:creator>
      <dc:date>2024-01-19T06:15:23Z</dc:date>
    </item>
    <item>
      <title>Re: ERR050481 on S32G274A-RDB2</title>
      <link>https://community.nxp.com/t5/S32G/ERR050481-on-S32G274A-RDB2/m-p/1792541#M5731</link>
      <description>&lt;P&gt;Hello,&amp;nbsp; @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225662" target="_blank"&gt;TudorMorosanu&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks for the question.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;In BSP29, the ERR050481 is only implemented in Linux, which is described in the user manual of BSP: “A workaround for the ERR050481 erratum has been included in kernel 5.4”&lt;/LI&gt;&lt;LI&gt;From BSP30, a workaround for the ERR050481 erratum has been included in Linux Kernel and TF-A(ARM trusted firmware).&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;From my opinion, it need to be also implemented in QNX in order to avoid any issues that may cause by the tlbiva* operation in your system.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jan 2024 02:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/ERR050481-on-S32G274A-RDB2/m-p/1792541#M5731</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-01-22T02:37:42Z</dc:date>
    </item>
    <item>
      <title>Re: ERR050481 on S32G274A-RDB2</title>
      <link>https://community.nxp.com/t5/S32G/ERR050481-on-S32G274A-RDB2/m-p/1792823#M5744</link>
      <description>&lt;P&gt;Thank you very much!&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jan 2024 09:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/ERR050481-on-S32G274A-RDB2/m-p/1792823#M5744</guid>
      <dc:creator>TudorMorosanu</dc:creator>
      <dc:date>2024-01-22T09:09:05Z</dc:date>
    </item>
  </channel>
</rss>