<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32G 274A gpio button SDA_GPIO0</title>
    <link>https://community.nxp.com/t5/S32G/S32G-274A-gpio-button-SDA-GPIO0/m-p/1419248#M567</link>
    <description>&lt;P&gt;Hi list,&lt;/P&gt;&lt;P&gt;I'm using a s32g274a-evb and i try to use the button available on the mother board S32GRV-PLATEVB.&lt;/P&gt;&lt;P&gt;The document SCH-30081 (Rev D.) describes on the OpenSDA Interface's page (the 20th) a button&amp;nbsp; available which could be configured with the jumper J67 (position 2-3) to i quote "enable button when OpenSDA is not powered".&lt;/P&gt;&lt;P&gt;What does that means? Can i use this button connected on that gpio accessible through /sys/kernel/debug/gpio?&lt;/P&gt;&lt;P&gt;I seems that this button is accessible through *SDA_GPIO0* but i don't see any connection to the chip (as opposite of SDA_GPIO0_B..)&lt;/P&gt;&lt;P&gt;I use the kernel branch *tags/bsp31.0-5.4-rt* with the configuration created by *s32gen1_defconfig* and the dtb file *fsl-s32g2xxa-evb.dtb*.&lt;/P&gt;&lt;P&gt;Is it the right dtb for the manipulation? Should i use an other dtb or modify the current one to support the button connected to this gpio?&lt;/P&gt;&lt;P&gt;Let me know if you already try this setting.&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
    <pubDate>Thu, 24 Feb 2022 16:51:07 GMT</pubDate>
    <dc:creator>jjp</dc:creator>
    <dc:date>2022-02-24T16:51:07Z</dc:date>
    <item>
      <title>S32G 274A gpio button SDA_GPIO0</title>
      <link>https://community.nxp.com/t5/S32G/S32G-274A-gpio-button-SDA-GPIO0/m-p/1419248#M567</link>
      <description>&lt;P&gt;Hi list,&lt;/P&gt;&lt;P&gt;I'm using a s32g274a-evb and i try to use the button available on the mother board S32GRV-PLATEVB.&lt;/P&gt;&lt;P&gt;The document SCH-30081 (Rev D.) describes on the OpenSDA Interface's page (the 20th) a button&amp;nbsp; available which could be configured with the jumper J67 (position 2-3) to i quote "enable button when OpenSDA is not powered".&lt;/P&gt;&lt;P&gt;What does that means? Can i use this button connected on that gpio accessible through /sys/kernel/debug/gpio?&lt;/P&gt;&lt;P&gt;I seems that this button is accessible through *SDA_GPIO0* but i don't see any connection to the chip (as opposite of SDA_GPIO0_B..)&lt;/P&gt;&lt;P&gt;I use the kernel branch *tags/bsp31.0-5.4-rt* with the configuration created by *s32gen1_defconfig* and the dtb file *fsl-s32g2xxa-evb.dtb*.&lt;/P&gt;&lt;P&gt;Is it the right dtb for the manipulation? Should i use an other dtb or modify the current one to support the button connected to this gpio?&lt;/P&gt;&lt;P&gt;Let me know if you already try this setting.&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 16:51:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-274A-gpio-button-SDA-GPIO0/m-p/1419248#M567</guid>
      <dc:creator>jjp</dc:creator>
      <dc:date>2022-02-24T16:51:07Z</dc:date>
    </item>
  </channel>
</rss>