<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32G-VNP-RDB2 LLCE_LINFlexD LINFlexD</title>
    <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LLCE-LINFlexD-LINFlexD/m-p/1778655#M5587</link>
    <description>&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;First of all, let's confirm the following questions:&lt;/P&gt;&lt;P&gt;1. Does LLCE_LINFlexD_x in this document refer to LLCE_LIN_x?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ki7691r0.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255512i3D29DCA8FF63027F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ki7691r0.bmp" alt="ki7691r0.bmp" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ki7691r0.bmp&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; 2. In this document, LINFlexD_x indicates LINFlexD_0(uart0), LINFlexD_1(uart1), and LINFlexD_2?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xpf2s1kw.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255513iB0910AD56BABE0BB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xpf2s1kw.bmp" alt="xpf2s1kw.bmp" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xpf2s1kw.bmp&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;3. Next is their drive&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1bje6du8.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255514iD44AD05E1BB33FE8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1bje6du8.bmp" alt="1bje6du8.bmp" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1bje6du8.bmp&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;Whose driver is this fsl linflexuart.c file?&lt;/P&gt;&lt;P&gt;If it is the driver of LLCE_LINFlexD_x, then the driver mentions DMA sending and receiving data, while LLCE_LINFlexD_x mentions that DMA cannot be used. If not, can you provide the driver of LLCE_LINFlexD_x?&lt;/P&gt;&lt;P&gt;If it is a driver of LINFlexD_x, can this driver be used to implement LIN as a master-slave mode to send data on linux? This seems to be through the uart mode to achieve data sending and receiving.&lt;/P&gt;&lt;P&gt;At present, we mainly want to transfer the data transmission of LIN master-slave mode of M core to A core in linux, but there seems to be a problem in the driver. In addition, we planned to use LINFlexD_x at the beginning, but worried about the conflict between LINFlexD_0 and uart0, so we are considering using it now LLCE_LINFlexD_1 to implement.&lt;/P&gt;&lt;P&gt;Your help would be greatly appreciated.&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
    <pubDate>Thu, 21 Dec 2023 09:56:13 GMT</pubDate>
    <dc:creator>StanleyShen</dc:creator>
    <dc:date>2023-12-21T09:56:13Z</dc:date>
    <item>
      <title>S32G-VNP-RDB2 LLCE_LINFlexD LINFlexD</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LLCE-LINFlexD-LINFlexD/m-p/1778655#M5587</link>
      <description>&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;First of all, let's confirm the following questions:&lt;/P&gt;&lt;P&gt;1. Does LLCE_LINFlexD_x in this document refer to LLCE_LIN_x?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ki7691r0.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255512i3D29DCA8FF63027F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ki7691r0.bmp" alt="ki7691r0.bmp" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ki7691r0.bmp&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; 2. In this document, LINFlexD_x indicates LINFlexD_0(uart0), LINFlexD_1(uart1), and LINFlexD_2?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xpf2s1kw.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255513iB0910AD56BABE0BB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xpf2s1kw.bmp" alt="xpf2s1kw.bmp" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xpf2s1kw.bmp&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;3. Next is their drive&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1bje6du8.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255514iD44AD05E1BB33FE8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="1bje6du8.bmp" alt="1bje6du8.bmp" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1bje6du8.bmp&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;Whose driver is this fsl linflexuart.c file?&lt;/P&gt;&lt;P&gt;If it is the driver of LLCE_LINFlexD_x, then the driver mentions DMA sending and receiving data, while LLCE_LINFlexD_x mentions that DMA cannot be used. If not, can you provide the driver of LLCE_LINFlexD_x?&lt;/P&gt;&lt;P&gt;If it is a driver of LINFlexD_x, can this driver be used to implement LIN as a master-slave mode to send data on linux? This seems to be through the uart mode to achieve data sending and receiving.&lt;/P&gt;&lt;P&gt;At present, we mainly want to transfer the data transmission of LIN master-slave mode of M core to A core in linux, but there seems to be a problem in the driver. In addition, we planned to use LINFlexD_x at the beginning, but worried about the conflict between LINFlexD_0 and uart0, so we are considering using it now LLCE_LINFlexD_1 to implement.&lt;/P&gt;&lt;P&gt;Your help would be greatly appreciated.&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 09:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LLCE-LINFlexD-LINFlexD/m-p/1778655#M5587</guid>
      <dc:creator>StanleyShen</dc:creator>
      <dc:date>2023-12-21T09:56:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32G-VNP-RDB2 LLCE_LINFlexD LINFlexD</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LLCE-LINFlexD-LINFlexD/m-p/1787313#M5663</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;1 and 2 yes, for 3)&lt;/P&gt;
&lt;P&gt;it will work as Slave node too, but to follow LIN standard this pullup should be removed. You can just solder out R4 and place header to have this configurable.&lt;BR /&gt;Yes, there is no LIN driver in the SDK. You can find simple baremetal code for LIN in S32DS called "linflex_lin".&lt;/P&gt;
&lt;P&gt;&amp;nbsp;yes, the LIN transceiver requires 12 V supply on pin P3.3&lt;/P&gt;
&lt;P&gt;or receiving data be sure CANoe is set to respond on given ID and check the RX frame on bus with the scope too.&lt;/P&gt;
&lt;P&gt;You can refer to master/slave example on&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5748G-LINFlex-LIN-Master-Slave-test-GHS616/ta-p/1117197" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5748G-LINFlex-LIN-Master-Slave-test-GHS616/ta-p/1117197&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jan 2024 15:06:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LLCE-LINFlexD-LINFlexD/m-p/1787313#M5663</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-01-11T15:06:06Z</dc:date>
    </item>
  </channel>
</rss>