<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックKeep uboot GPIO settings through kernel boot S32G2</title>
    <link>https://community.nxp.com/t5/S32G/Keep-uboot-GPIO-settings-through-kernel-boot-S32G2/m-p/1778166#M5575</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd like to configure a GPIO in u-boot, then tell the kernel to ignore that GPIO during boot. The kernel currently overrides the u-boot settings. I added the specific GPIO to the gpio-reserved-ranges in the DTS but that had no effect. I currently do not have anything in the DTS file to configure this specific GPIO.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 20 Dec 2023 21:10:14 GMT</pubDate>
    <dc:creator>lodo1234</dc:creator>
    <dc:date>2023-12-20T21:10:14Z</dc:date>
    <item>
      <title>Keep uboot GPIO settings through kernel boot S32G2</title>
      <link>https://community.nxp.com/t5/S32G/Keep-uboot-GPIO-settings-through-kernel-boot-S32G2/m-p/1778166#M5575</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd like to configure a GPIO in u-boot, then tell the kernel to ignore that GPIO during boot. The kernel currently overrides the u-boot settings. I added the specific GPIO to the gpio-reserved-ranges in the DTS but that had no effect. I currently do not have anything in the DTS file to configure this specific GPIO.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 20 Dec 2023 21:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Keep-uboot-GPIO-settings-through-kernel-boot-S32G2/m-p/1778166#M5575</guid>
      <dc:creator>lodo1234</dc:creator>
      <dc:date>2023-12-20T21:10:14Z</dc:date>
    </item>
    <item>
      <title>Re: Keep uboot GPIO settings through kernel boot S32G2</title>
      <link>https://community.nxp.com/t5/S32G/Keep-uboot-GPIO-settings-through-kernel-boot-S32G2/m-p/1780911#M5603</link>
      <description>&lt;P&gt;Hi Gabriel LoDolce&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well&lt;/P&gt;
&lt;P&gt;I think you have to disable that gpio in kernal which reconfigs. We suggest you please go with u-boot and kernel community for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards ,&lt;/P&gt;
&lt;P&gt;Tushar&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Dec 2023 12:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Keep-uboot-GPIO-settings-through-kernel-boot-S32G2/m-p/1780911#M5603</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2023-12-28T12:50:44Z</dc:date>
    </item>
  </channel>
</rss>