<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flash sja1110 non volatile memory command line in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1777068#M5558</link>
    <description>Hi Abdullah,&lt;BR /&gt;I see that this tool is only for windows env. However I'm interesting to work with linux env ( ubuntu 20.04) so,Is there sopport from NXP to flash SJA11110 non-volatile-memory using pemicro debug probe?</description>
    <pubDate>Tue, 19 Dec 2023 09:38:26 GMT</pubDate>
    <dc:creator>cristianchacha</dc:creator>
    <dc:date>2023-12-19T09:38:26Z</dc:date>
    <item>
      <title>Flash sja1110 non volatile memory command line</title>
      <link>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1766735#M5478</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm user of S32 Desing Studio. I use a p&amp;amp;e micro device to flash sja1110, I achieve flash with GUI using Debug_FLASH files and ISSI_IS25LQ040D_1x32x128k_SJA1110.arp in config degub_flash_pnemicro.&lt;BR /&gt;&lt;BR /&gt;I would likte to reproduce this using CLI, for automatic flashing , it's possible? . My goal is flash in non-volatile memory to avoid flash againg after power off the board.&lt;BR /&gt;&lt;BR /&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 20:13:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1766735#M5478</guid>
      <dc:creator>cristianchacha</dc:creator>
      <dc:date>2023-11-30T20:13:56Z</dc:date>
    </item>
    <item>
      <title>Re: Flash sja1110 non volatile memory command line</title>
      <link>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1772323#M5527</link>
      <description>&lt;P&gt;Hi Cristianchacha,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you using the SJA1110 EVM or do you have a customized board?&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are using SJA1110 EVM, then you can use our python tools for&amp;nbsp;&lt;/P&gt;&lt;P&gt;flashing the firmware in the non-volatile memory(Flash). You need to&amp;nbsp;&lt;/P&gt;&lt;P&gt;download our EVB Host tools for that, if you already have not done that.&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&amp;nbsp;&lt;BR /&gt;Abdullah&lt;/P&gt;</description>
      <pubDate>Mon, 11 Dec 2023 13:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1772323#M5527</guid>
      <dc:creator>abdullahzafar</dc:creator>
      <dc:date>2023-12-11T13:20:28Z</dc:date>
    </item>
    <item>
      <title>Re: Flash sja1110 non volatile memory command line</title>
      <link>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1772344#M5528</link>
      <description>&lt;P&gt;Hello Abdullah,&lt;BR /&gt;&lt;BR /&gt;I'm using a custom board, we use a pemicro to load in RAM, but I would like to load in non-volatile memory,.I see that python script is design to load over USB , but I'm not sure how can I procudure.&lt;/P&gt;&lt;P&gt;BR,&lt;BR /&gt;Cristian&lt;/P&gt;</description>
      <pubDate>Mon, 11 Dec 2023 14:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1772344#M5528</guid>
      <dc:creator>cristianchacha</dc:creator>
      <dc:date>2023-12-11T14:03:24Z</dc:date>
    </item>
    <item>
      <title>Re: Flash sja1110 non volatile memory command line</title>
      <link>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1772889#M5532</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;cristianchacha,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Python tools can be used for flashing the SRAM only. Regarding the CLI, I am not absolutely certain if that is possible. I would suggest you to contact PE micro or browse through their documentation.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;update:&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;you need to have PROGACMP: &lt;A href="https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320181&amp;amp;productTab=5053" target="_blank"&gt;https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320181&amp;amp;productTab=5053&lt;/A&gt; in order to use CLI.&lt;/P&gt;
&lt;P&gt;UG can be found here: &lt;A href="https://cdn.accentuate.io/4611531898947/11479159308355/CPROGACMP-User-Guide-v1608126976405.pdf" target="_blank"&gt;https://cdn.accentuate.io/4611531898947/11479159308355/CPROGACMP-User-Guide-v1608126976405.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Abdullah&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Dec 2023 07:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1772889#M5532</guid>
      <dc:creator>abdullahzafar</dc:creator>
      <dc:date>2023-12-12T07:48:00Z</dc:date>
    </item>
    <item>
      <title>Re: Flash sja1110 non volatile memory command line</title>
      <link>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1777068#M5558</link>
      <description>Hi Abdullah,&lt;BR /&gt;I see that this tool is only for windows env. However I'm interesting to work with linux env ( ubuntu 20.04) so,Is there sopport from NXP to flash SJA11110 non-volatile-memory using pemicro debug probe?</description>
      <pubDate>Tue, 19 Dec 2023 09:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1777068#M5558</guid>
      <dc:creator>cristianchacha</dc:creator>
      <dc:date>2023-12-19T09:38:26Z</dc:date>
    </item>
    <item>
      <title>Re: Flash sja1110 non volatile memory command line</title>
      <link>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1777179#M5560</link>
      <description>&lt;P&gt;Hi cristianchacha,&amp;nbsp;&lt;/P&gt;&lt;P&gt;PE micro needs to be contacted to see if they have such a tool.&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Abdullah&lt;/P&gt;</description>
      <pubDate>Tue, 19 Dec 2023 12:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Flash-sja1110-non-volatile-memory-command-line/m-p/1777179#M5560</guid>
      <dc:creator>abdullahzafar</dc:creator>
      <dc:date>2023-12-19T12:01:55Z</dc:date>
    </item>
  </channel>
</rss>