<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: inport hex file in SD32 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/inport-hex-file-in-SD32/m-p/1753269#M5238</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222720"&gt;@cristianchacha&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The hex file contains the configuration which is loaded into the Switch SRAM however, it does not show/display the configuration in SDK GUI. For this purpose you need to have the .mex file, which is used by the GUI to display the configuration in the user interface.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Sabeur&lt;/P&gt;</description>
    <pubDate>Tue, 07 Nov 2023 06:09:05 GMT</pubDate>
    <dc:creator>Sabeur</dc:creator>
    <dc:date>2023-11-07T06:09:05Z</dc:date>
    <item>
      <title>inport hex file in SD32</title>
      <link>https://community.nxp.com/t5/S32G/inport-hex-file-in-SD32/m-p/1747930#M5160</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using S32Design studio to load a hex file.&lt;/P&gt;&lt;P&gt;the input hex file is specific for SJA1110 switch , this hex file has a TABLE ID = 8 (L2 forwarding table) information, with all port activate, however every time that i load this values in S32 Design studio , the L2 forwarding table is cleared.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cristianchacha_0-1698419617660.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/247262iF75699B796329F26/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cristianchacha_0-1698419617660.png" alt="cristianchacha_0-1698419617660.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Oct 2023 15:13:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/inport-hex-file-in-SD32/m-p/1747930#M5160</guid>
      <dc:creator>cristianchacha</dc:creator>
      <dc:date>2023-10-27T15:13:48Z</dc:date>
    </item>
    <item>
      <title>Re: inport hex file in SD32</title>
      <link>https://community.nxp.com/t5/S32G/inport-hex-file-in-SD32/m-p/1753269#M5238</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222720"&gt;@cristianchacha&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The hex file contains the configuration which is loaded into the Switch SRAM however, it does not show/display the configuration in SDK GUI. For this purpose you need to have the .mex file, which is used by the GUI to display the configuration in the user interface.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Sabeur&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 06:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/inport-hex-file-in-SD32/m-p/1753269#M5238</guid>
      <dc:creator>Sabeur</dc:creator>
      <dc:date>2023-11-07T06:09:05Z</dc:date>
    </item>
    <item>
      <title>Re: inport hex file in SD32</title>
      <link>https://community.nxp.com/t5/S32G/inport-hex-file-in-SD32/m-p/1757747#M5310</link>
      <description>&lt;P&gt;I see that when I added the hex file, all configuration is show in GUI, however L2 forwarding table is cleared, so import a hex file modify the .mex, right ? so I think this option is not generate properly the .mex, is this possible ??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you support me with specific way to use .hex files ? or how can I procedure ?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 16:01:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/inport-hex-file-in-SD32/m-p/1757747#M5310</guid>
      <dc:creator>cristianchacha</dc:creator>
      <dc:date>2023-11-15T16:01:50Z</dc:date>
    </item>
    <item>
      <title>Re: inport hex file in SD32</title>
      <link>https://community.nxp.com/t5/S32G/inport-hex-file-in-SD32/m-p/1758365#M5332</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I confirm this is an issue with the latest SDK and S32DS3.5. The hex file seems to be correct. Still importing does not work.&lt;/P&gt;&lt;P&gt;This should be fixed with the next SDK release.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Sabeur&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 13:00:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/inport-hex-file-in-SD32/m-p/1758365#M5332</guid>
      <dc:creator>Sabeur</dc:creator>
      <dc:date>2023-11-16T13:00:10Z</dc:date>
    </item>
  </channel>
</rss>