<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CPU:1 failed to come online error in S32G</title>
    <link>https://community.nxp.com/t5/S32G/CPU-1-failed-to-come-online-error/m-p/1303833#M52</link>
    <description>&lt;P&gt;Sorry but the information you provided is too vague. S32G275 is a non-existent&lt;BR /&gt;part number. Furthermore, there are multiple development systems and reference &lt;BR /&gt;designs built around S32G2 processors . Without knowing the exact processor and&lt;BR /&gt;board model you are working with, the only suggestion I can share is as follows.&lt;BR /&gt;If your hardware is one of the original NXP development or reference boards, &lt;BR /&gt;use boot images generated with the most recent automotive BSP. You can build &lt;BR /&gt;them locally or use pre-built ones. There are no known issues with multiple &lt;BR /&gt;cores startup in the default BSP configuration of u-Boot, Linux an the default DTB.&lt;/P&gt;
&lt;P&gt;The most recent Automotive BSP can be obtained by following &lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32G2-REFSW-D" target="_self"&gt;this link&lt;/A&gt;. Refer to the BSP User Manual for more details. &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon.&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jul 2021 09:14:21 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2021-07-07T09:14:21Z</dc:date>
    <item>
      <title>CPU:1 failed to come online error</title>
      <link>https://community.nxp.com/t5/S32G/CPU-1-failed-to-come-online-error/m-p/1302474#M48</link>
      <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;I am working on S32G275a eval board. During linux booting time i am getting following errors.&lt;/P&gt;&lt;P&gt;[ 1.089224] CPU1: failed to come online&lt;BR /&gt;[ 1.092715] CPU1: failed in unknown state : 0x0&lt;BR /&gt;[ 2.150398] CPU2: failed to come online&lt;BR /&gt;[ 2.153880] CPU2: failed in unknown state : 0x0&lt;BR /&gt;[ 3.211563] CPU3: failed to come online&lt;BR /&gt;[ 3.215045] CPU3: failed in unknown state : 0x0&lt;/P&gt;&lt;P&gt;I am able to boot with primary cpu only. But other cpus are failed to boot. Even through sysfs entries also i am not able to make them online.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you help me on how to resolve this issue.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jul 2021 13:17:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/CPU-1-failed-to-come-online-error/m-p/1302474#M48</guid>
      <dc:creator>VB13</dc:creator>
      <dc:date>2021-07-05T13:17:42Z</dc:date>
    </item>
    <item>
      <title>Re: CPU:1 failed to come online error</title>
      <link>https://community.nxp.com/t5/S32G/CPU-1-failed-to-come-online-error/m-p/1303009#M50</link>
      <description>&lt;P&gt;This problem description is missing important details:&lt;/P&gt;
&lt;P&gt;1. The type of NXP development board you are working with&lt;/P&gt;
&lt;P&gt;2. The version of Automotive BSP being used, if at all.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 08:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/CPU-1-failed-to-come-online-error/m-p/1303009#M50</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-07-06T08:51:34Z</dc:date>
    </item>
    <item>
      <title>Re: CPU:1 failed to come online error</title>
      <link>https://community.nxp.com/t5/S32G/CPU-1-failed-to-come-online-error/m-p/1303021#M51</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;s32g275 eval board with bsp 25.0. The following entries are present in dts file.&lt;/P&gt;&lt;P&gt;cpu2: cpu@100 {&lt;BR /&gt;device_type = "cpu";&lt;BR /&gt;compatible = "arm,cortex-a53";&lt;BR /&gt;reg = &amp;lt;0x0 0x100&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;cpu3: cpu@101 {&lt;BR /&gt;device_type = "cpu";&lt;BR /&gt;compatible = "arm,cortex-a53";&lt;BR /&gt;reg = &amp;lt;0x0 0x101&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Here i did'nt see enable methods either PCI or SPINTABLE. I am not sure whether this can be the reason for this issue. At u-boot side i am able to see all cpus are up. Kindly let me know whether this issue can be fixed at u-boot or at linux.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Balaji.V&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 09:04:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/CPU-1-failed-to-come-online-error/m-p/1303021#M51</guid>
      <dc:creator>VB13</dc:creator>
      <dc:date>2021-07-06T09:04:30Z</dc:date>
    </item>
    <item>
      <title>Re: CPU:1 failed to come online error</title>
      <link>https://community.nxp.com/t5/S32G/CPU-1-failed-to-come-online-error/m-p/1303833#M52</link>
      <description>&lt;P&gt;Sorry but the information you provided is too vague. S32G275 is a non-existent&lt;BR /&gt;part number. Furthermore, there are multiple development systems and reference &lt;BR /&gt;designs built around S32G2 processors . Without knowing the exact processor and&lt;BR /&gt;board model you are working with, the only suggestion I can share is as follows.&lt;BR /&gt;If your hardware is one of the original NXP development or reference boards, &lt;BR /&gt;use boot images generated with the most recent automotive BSP. You can build &lt;BR /&gt;them locally or use pre-built ones. There are no known issues with multiple &lt;BR /&gt;cores startup in the default BSP configuration of u-Boot, Linux an the default DTB.&lt;/P&gt;
&lt;P&gt;The most recent Automotive BSP can be obtained by following &lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32G2-REFSW-D" target="_self"&gt;this link&lt;/A&gt;. Refer to the BSP User Manual for more details. &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jul 2021 09:14:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/CPU-1-failed-to-come-online-error/m-p/1303833#M52</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-07-07T09:14:21Z</dc:date>
    </item>
  </channel>
</rss>