<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: Running ELF on M7_0  Core on S32G-VNP-RDB3</title>
    <link>https://community.nxp.com/t5/S32G/Running-ELF-on-M7-0-Core-on-S32G-VNP-RDB3/m-p/1746218#M5141</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We can recommend looking into the "Software Enablement Guide/Training" available under the RDB3 product page (link:&amp;nbsp;&lt;A href="https://www.nxp.com/design/designs/s32g3-vehicle-networking-reference-design:S32G-VNP-RDB3" target="_blank"&gt;S32G3 Vehicle Networking Reference Design | NXP Semiconductors&lt;/A&gt;).&lt;/P&gt;
&lt;P&gt;This provides the usage of an external memory interface for booting the platform.&lt;/P&gt;
&lt;P&gt;As for loading the binaries from Linux, this flow is not recommended since it is not documented officially. There is an example that loads the binaries from uboot (IPCF_Example_S32G399_M7_0) but it is specific to that example. Modifications are required if you are willing to load additional/different binaries.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Wed, 25 Oct 2023 18:09:50 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2023-10-25T18:09:50Z</dc:date>
    <item>
      <title>Running ELF on M7_0  Core on S32G-VNP-RDB3</title>
      <link>https://community.nxp.com/t5/S32G/Running-ELF-on-M7-0-Core-on-S32G-VNP-RDB3/m-p/1745492#M5131</link>
      <description>&lt;P&gt;Dear NXP Support,&amp;nbsp;&lt;/P&gt;&lt;P&gt;We recently purchased the &lt;STRONG&gt;S32G-VNP-RDB3&lt;/STRONG&gt; Board and have successfully compiled the &lt;STRONG&gt;Siul2_Dio_ToggleLed_S32G399A_M7.elf&lt;/STRONG&gt; example using S32 Design Studio for M7_0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please provide guidance on the steps necessary to transfer this ELF file and execute it on the M7_0 Core on the S32G-VNP-RDB3 Board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently, we do not have the Lauterbach or S32G Debug Probe debugger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there an alternative method for transferring and executing, for example, the Siul2_Dio_ToggleLed_S32G399A_M7.elf, using an SD Card or the Flash tool with the COM Port and running it on the M7_0 Core?&lt;/P&gt;&lt;P&gt;Alternatively, is there a way to load it via Linux that's running on the SD Card?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please provide any documentation needed to describe this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note: We successfully ran the included SD Card that was in the kit, and we could boot Linux on A53.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Tue, 24 Oct 2023 22:57:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Running-ELF-on-M7-0-Core-on-S32G-VNP-RDB3/m-p/1745492#M5131</guid>
      <dc:creator>s153022</dc:creator>
      <dc:date>2023-10-24T22:57:44Z</dc:date>
    </item>
    <item>
      <title>Re: Running ELF on M7_0  Core on S32G-VNP-RDB3</title>
      <link>https://community.nxp.com/t5/S32G/Running-ELF-on-M7-0-Core-on-S32G-VNP-RDB3/m-p/1746218#M5141</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;We can recommend looking into the "Software Enablement Guide/Training" available under the RDB3 product page (link:&amp;nbsp;&lt;A href="https://www.nxp.com/design/designs/s32g3-vehicle-networking-reference-design:S32G-VNP-RDB3" target="_blank"&gt;S32G3 Vehicle Networking Reference Design | NXP Semiconductors&lt;/A&gt;).&lt;/P&gt;
&lt;P&gt;This provides the usage of an external memory interface for booting the platform.&lt;/P&gt;
&lt;P&gt;As for loading the binaries from Linux, this flow is not recommended since it is not documented officially. There is an example that loads the binaries from uboot (IPCF_Example_S32G399_M7_0) but it is specific to that example. Modifications are required if you are willing to load additional/different binaries.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Oct 2023 18:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Running-ELF-on-M7-0-Core-on-S32G-VNP-RDB3/m-p/1746218#M5141</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-10-25T18:09:50Z</dc:date>
    </item>
  </channel>
</rss>