<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: llce-core debugfs issue based on BSP38 release on S32G RDB3</title>
    <link>https://community.nxp.com/t5/S32G/llce-core-debugfs-issue-based-on-BSP38-release-on-S32G-RDB3/m-p/1742306#M5085</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This seems to be a known issue. The following workaround is being shown:&lt;/P&gt;
&lt;P&gt;"CORES_TS_OFFSET must be set to 0x13730."&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Wed, 18 Oct 2023 18:09:48 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2023-10-18T18:09:48Z</dc:date>
    <item>
      <title>llce-core debugfs issue based on BSP38 release on S32G RDB3</title>
      <link>https://community.nxp.com/t5/S32G/llce-core-debugfs-issue-based-on-BSP38-release-on-S32G-RDB3/m-p/1742089#M5083</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tested llce related features recectly based on SDK BSP38 release, but the following issue happened when I followed section "12.3.4.1 Fault detection counters" of the BSP38 user manual for S32G3 platforms:&lt;/P&gt;&lt;P&gt;root@s32g399ardb3:~# ls /sys/kernel/debug/llce_core/core1_ts&lt;BR /&gt;/sys/kernel/debug/llce_core/core1_ts&lt;BR /&gt;root@s32g399ardb3:~# cat /sys/kernel/debug/llce_core/core1_ts&lt;BR /&gt;[ 8.904090] s32cc-dwmac 4033c000.ethernet eth0: PHY [stmmac-0:01] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)&lt;BR /&gt;[ 8.905089] s32cc-dwmac 4033c000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0&lt;BR /&gt;[ 8.907652] s32cc-dwmac 4033c000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-1&lt;BR /&gt;[ 8.910500] s32cc-dwmac 4033c000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-2&lt;BR /&gt;[ 8.913133] s32cc-dwmac 4033c000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-3&lt;BR /&gt;[ 8.915952] s32cc-dwmac 4033c000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-4&lt;BR /&gt;[ 8.925449] s32cc-dwmac 4033c000.ethernet eth0: Enabling Safety Features&lt;BR /&gt;[ 8.925551] s32cc-dwmac 4033c000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported&lt;BR /&gt;[ 8.925832] s32cc-dwmac 4033c000.ethernet eth0: registered PTP clock&lt;BR /&gt;[ 8.926250] s32cc-dwmac 4033c000.ethernet eth0: FPE workqueue start&lt;BR /&gt;[ 8.926259] s32cc-dwmac 4033c000.ethernet eth0: configuring for phy/rgmii-id link mode&lt;BR /&gt;[ 8.929065] 8021q: adding VLAN 0 to HW filter on device eth0&lt;BR /&gt;[ 26.275118] Unable to handle kernel paging request at virtual address ffffffc00bb50870&lt;BR /&gt;[ 26.371260] Mem abort info:&lt;BR /&gt;[ 26.374038] ESR = 0x0000000096000007&lt;BR /&gt;[ 26.377763] EC = 0x25: DABT (current EL), IL = 32 bits&lt;BR /&gt;[ 26.383060] SET = 0, FnV = 0&lt;BR /&gt;[ 26.386094] EA = 0, S1PTW = 0&lt;BR /&gt;[ 26.389204] FSC = 0x07: level 3 translation fault&lt;BR /&gt;[ 26.394076] Data abort info:&lt;BR /&gt;[ 26.396930] ISV = 0, ISS = 0x00000007&lt;BR /&gt;[ 26.400765] CM = 0, WnR = 0&lt;BR /&gt;[ 26.403711] swapper pgtable: 4k pages, 39-bit VAs, pgdp=0000000080bc4000&lt;BR /&gt;[ 26.410394] [ffffffc00bb50870] pgd=10000008dffff003, p4d=10000008dffff003, pud=10000008dffff003, pmd=1000000880964003, pte=0000000000000000&lt;BR /&gt;[ 26.422895] Internal error: Oops: 96000007 [#1] PREEMPT SMP&lt;BR /&gt;[ 26.428439] Modules linked in: sja1110(O) llce_can llce_mailbox llce_core&lt;BR /&gt;[ 26.435211] CPU: 5 PID: 332 Comm: cat Tainted: G O 5.15.119-rt65+ge18f05316cd9 #1&lt;BR /&gt;[ 26.443977] Hardware name: NXP S32G399A-RDB3 (DT)&lt;BR /&gt;[ 26.448664] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)&lt;BR /&gt;[ 26.455606] pc : debugfs_readl_get+0x4/0x30 [llce_core]&lt;BR /&gt;[ 26.460814] lr : simple_attr_read+0x6c/0x11c&lt;BR /&gt;[ 26.465068] sp : ffffffc00beb3d00&lt;BR /&gt;[ 26.468366] x29: ffffffc00beb3d00 x28: ffffff8801509040 x27: 0000000000000000&lt;BR /&gt;[ 26.475483] x26: 0000000000000000 x25: 0000000000000000 x24: 0000007f9e81f000&lt;BR /&gt;[ 26.482601] x23: 0000000000020000 x22: ffffff8805422250 x21: 0000000000000000&lt;BR /&gt;[ 26.489719] x20: ffffffc00beb3df0 x19: ffffff8805422200 x18: 0000000000000000&lt;BR /&gt;[ 26.496836] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000000&lt;BR /&gt;[ 26.503954] x14: 0000000000000000 x13: 0000000000000000 x12: 0000000000000000&lt;BR /&gt;[ 26.511071] x11: 0000000000000000 x10: 0000000000000000 x9 : 0000000000000000&lt;BR /&gt;[ 26.518189] x8 : 0000000000000000 x7 : 0000000000000000 x6 : 0000000000000000&lt;BR /&gt;[ 26.525306] x5 : 0000000000000000 x4 : 0000000000000000 x3 : ffffff8805422250&lt;BR /&gt;[ 26.532424] x2 : ffffffc0008d0000 x1 : ffffffc00beb3d40 x0 : ffffffc00bb50870&lt;BR /&gt;[ 26.539542] Call trace:&lt;BR /&gt;[ 26.541975] debugfs_readl_get+0x4/0x30 [llce_core]&lt;BR /&gt;[ 26.546833] debugfs_attr_read+0x4c/0x94&lt;BR /&gt;[ 26.550740] vfs_read+0x90/0x1b0&lt;BR /&gt;[ 26.553951] ksys_read+0x68/0xf4&lt;BR /&gt;[ 26.557162] __arm64_sys_read+0x1c/0x2c&lt;BR /&gt;[ 26.560982] invoke_syscall+0x48/0x114&lt;BR /&gt;[ 26.564714] el0_svc_common.constprop.0+0x44/0xfc&lt;BR /&gt;[ 26.569401] do_el0_svc+0x28/0xa0&lt;BR /&gt;[ 26.572699] el0_svc+0x28/0x80&lt;BR /&gt;[ 26.575737] el0t_64_sync_handler+0xa4/0x130&lt;BR /&gt;[ 26.579991] el0t_64_sync+0x1a0/0x1a4&lt;BR /&gt;[ 26.583642] Code: bad PC value&lt;BR /&gt;[ 26.586678] ---[ end trace cd1c0c2028b64c60 ]---&lt;BR /&gt;[ 26.591374] printk: console [ttyLF0]: printing thread stopped&lt;/P&gt;&lt;P&gt;Message from syslogd@ at Thu Apr 28 17:42:45 2022 ...&lt;BR /&gt;: Code: bad PC value&lt;BR /&gt;Segmentation fault&lt;/P&gt;&lt;P&gt;Message from syslogd@ at Thu Apr 28 17:42:45 2022 ...&lt;BR /&gt;: Internal error: Oops: 96000007 [#1] PREEMPT SMP&lt;BR /&gt;&lt;A href="mailto:root@s32g399ardb3:~" target="_blank"&gt;root@s32g399ardb3:~#&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I attached the whole log.&lt;/P&gt;&lt;P&gt;And the LLCE firmware are v1.0.7.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Would you please help to check the issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Zhantao&lt;/P&gt;</description>
      <pubDate>Wed, 18 Oct 2023 11:52:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/llce-core-debugfs-issue-based-on-BSP38-release-on-S32G-RDB3/m-p/1742089#M5083</guid>
      <dc:creator>hittzt</dc:creator>
      <dc:date>2023-10-18T11:52:54Z</dc:date>
    </item>
    <item>
      <title>Re: llce-core debugfs issue based on BSP38 release on S32G RDB3</title>
      <link>https://community.nxp.com/t5/S32G/llce-core-debugfs-issue-based-on-BSP38-release-on-S32G-RDB3/m-p/1742306#M5085</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This seems to be a known issue. The following workaround is being shown:&lt;/P&gt;
&lt;P&gt;"CORES_TS_OFFSET must be set to 0x13730."&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Oct 2023 18:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/llce-core-debugfs-issue-based-on-BSP38-release-on-S32G-RDB3/m-p/1742306#M5085</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-10-18T18:09:48Z</dc:date>
    </item>
    <item>
      <title>Re: llce-core debugfs issue based on BSP38 release on S32G RDB3</title>
      <link>https://community.nxp.com/t5/S32G/llce-core-debugfs-issue-based-on-BSP38-release-on-S32G-RDB3/m-p/1742946#M5092</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205137"&gt;@Daniel-Aguirre&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Yes, you are right, it it a known issue, and the&amp;nbsp;&lt;SPAN&gt;0x13730 value can fix it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Zhantao&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Oct 2023 13:09:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/llce-core-debugfs-issue-based-on-BSP38-release-on-S32G-RDB3/m-p/1742946#M5092</guid>
      <dc:creator>hittzt</dc:creator>
      <dc:date>2023-10-19T13:09:02Z</dc:date>
    </item>
  </channel>
</rss>